cancel
Showing results for 
Search instead for 
Did you mean: 

Error: "Will not fit in region 'QUADSPI' " and " 'QUADSPI' overflowed by ... bytes "

LTech
Associate III

I have set up only three screens with some images, and it wont flash the target (simulator works fine) and I get two errors:

Error: " 'Extflashsection' will not fit in region 'QUADSPI' "

Error: " 'QUADSPI' overflowed by ... bytes "

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Clive1 (HNL)
Senior II

Ok, and how large is the definition for the loader region in the scatter file or linker script? Keil?

The linker tends to fail if it is given bad parameters, or you're simply trying to put more data than will physically fit in the device.

If you tell it that is has a 8MB device, 16 or 32MB of stuff will not fit.

LTech
Associate III

I've started a new project and added same images and screens and now it works...

SR.8
Associate II

hi, have solved that issue? i am new to this touch gfx. i need to know, is that the only way by creating a new project only we can solve this issue?