cancel
Showing results for 
Search instead for 
Did you mean: 

Dynamically Change the Button Label (Wildcard)

IMirz.1
Associate

Hello,

I am trying to change the button labels dynamically through wildcard buffers, but the labels are not updated at all,

Unicode::UnicodeChar txtBufferButton1[3];

Unicode::UnicodeChar txtBufferButton2[3];

 char* data = "abc";

//trying text label update (not working)

button1.setWildcardTextBuffer(txtBufferButton1);

Unicode::strncpy(txtBufferButton1, data , 3);

button1.invalidate();

//trying int value update (not working)

button2.setWildcardTextBuffer(txtBufferButton2);

Unicode::snprintf(txtBufferButton2, 3, "%d", 123);

button2.invalidate();

These buttons are defined as shown here:

button1.setBitmaps(Bitmap(BITMAP_BTN_BG_DEFAULT_ID), Bitmap(BITMAP_BTN_BG_SECONDARY_ID));

button1.setBitmapXY(0, 0);

button1.setWildcardText(TypedText(T_CPSELECTBUTTON1));

button1.setWildcardTextPosition(0, 25, 68, 68);

button1.setWildcardTextColors(touchgfx::Color::getColorFrom24BitRGB(255, 255, 255), touchgfx::Color::getColorFrom24BitRGB(255, 255, 255));

button1.setIconBitmaps(Bitmap(BITMAP_NO_ICON_ID), Bitmap(BITMAP_NO_ICON_ID));

button1.setIconXY(0, 0);

button1.setPosition(20, 100, 68, 68);

button1.setAction(flexButtonCallback);

and same for button2.

Any help would be greatly appreciated.

Regards

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
MM..1
Chief III

Button is two image object. When you need text use button with label ...