2019-03-18 2:17 AM
Hello All
I am trying to add a ClickListener to ScrollWheel in my project.
I am referring following link as a tutorial for the same
https://touchgfx.zendesk.com/hc/en-us/articles/360002825452-Mixins-and-ClickListener
But, even afer following the tutorial as it is, I am getting following compilation error:
error: no match for call to '(touchgfx::Callback<Screen1View, const touchgfx::ScrollWheel&, const touchgfx::ClickEvent&>) (Screen1View*, void (Screen1View::*)(const touchgfx::ScrollWheel&, const touchgfx::ClickEvent&))'
MyCallback(this, &Screen1View::MyCallbackHandler){}
I am inserting code snippet with this file:
Screen1View.cpp
#include <gui/screen1_screen/Screen1View.hpp>
#include "string.h"
#include "main.h"
extern UART_HandleTypeDef huart5;
Screen1View::Screen1View()
{
MyCallback(this, &Screen1View::MyCallbackHandler){}
}
void Screen1View::setupScreen()
{
scrollWheel1.setClickAction(MyCallback);
}
void Screen1View::tearDownScreen()
{
}Screen1View.hpp
#ifndef SCREEN1_VIEW_HPP
#define SCREEN1_VIEW_HPP
#include <gui_generated/screen1_screen/Screen1ViewBase.hpp>
#include <gui/screen1_screen/Screen1Presenter.hpp>
class Screen1View : public Screen1ViewBase
{
public:
Screen1View();
virtual ~Screen1View() {}
virtual void setupScreen();
virtual void tearDownScreen();
void scrollWheel1UpdateItem(CustomContainer1& item, int16_t itemIndex);
void scrollWheel2UpdateItem(CustomContainer2& item, int16_t itemIndex);
// virtual void handleClickEvent(const ClickEvent& evt);
// virtual void handleDragEvent(const DragEvent& drgevt);
void MyCallbackHandler(const ScrollWheel &scroll, const ClickEvent &e);
protected:
// Declaring callback type of box and clickEvent
touchgfx::Callback<Screen1View, const ScrollWheel&, const ClickEvent&> MyCallback;
};
template<class T>
class ClickListener : public T
{
public:
ClickListener() : T(), clickAction(0)
{
T::setTouchable(true);
};
virtual void handleClickEvent(const ClickEvent& event)
{
T::handleClickEvent(event);
if (clickAction && clickAction->isValid())
{
clickAction->execute(*this, event);
}
}
void setClickAction(GenericCallback< const T&, const ClickEvent& > callback)
{
clickAction = &callback;
}
protected:
touchgfx::GenericCallback<> *clickAction; ///< The callback to be executed when T is clicked
};
#endif // SCREEN1_VIEW_HPPPlease tell me if I am doing any mistake in following the tutorial
2019-04-03 1:31 AM
Hi @kvkhekale,
Are you still having troubles with this? Can you send me the project? I wouldn't rule out an error in the guide.
/Martin
2020-12-23 8:29 AM
This part:
Screen1View::Screen1View()
{
MyCallback(this, &Screen1View::MyCallbackHandler){}
}
should be written as:
Screen1View::Screen1View():
MyCallback(this, &Screen1View::MyCallbackHandler)
{
}
And that is it.