cancel
Showing results for 
Search instead for 
Did you mean: 

Can DMA2D Scale an image from (480*640) RGB565 to (480*800) RGB565?

MSale.1
Senior

Maybe someone from Touchgfx can help in this

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

Hi,

The scaling is only done through software, the DMA2D does not impact/improve it.

/Romain

View solution in original post

4 REPLIES 4
Tilen MAJERLE
ST Employee

DMA2D hardware has no scaling feature available.

Which STM32 family are you referring to?

@Tilen MAJERLE​ 

H7

but you have this in touchGFX. is it by software then without using DMA2D at all or by combination?

Better question is scaledImage optimized DMA2D in TouchGFX or not? Im too interested

Hi,

The scaling is only done through software, the DMA2D does not impact/improve it.

/Romain