cancel
Showing results for 
Search instead for 
Did you mean: 

The SBSFU porting of STM32G431C8

PSui.1
Associate II

Due to cost constraints, only STM32G431x8 (64K byte flash memory) can be used, but there is no sample source code for G431x8 in the SBSFU library. I tried to port such a project, but I was a little confused.

1. The compilation of the 1_Image_SBSFU project of NUCLEO-G474RE is close to 50K bytes, which is not acceptable. But UM2262 didn't teach me how to delete some functions to reduce the size.

2. Maybe I can use NUCLEO-G031K8 to port, because its 1_Image_SBSFU project compiles only 36K bytes, but it is m0 core so I ca n’t determine whether it can be ported.

Any suggestions are greatly appreciated!

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
PSui.1
Associate II

Due to the different architectures of the core, flash ROM (single bank / dual bank), RAM (with or without CCMSRAM), it seems that it cannot be easily ported