cancel
Showing results for 
Search instead for 
Did you mean: 

RDP - Readout Protection on STM32F10x

hrobinson
Associate II
Posted on November 10, 2014 at 15:03

Hi,

I'm having a problem with the CMSIS peripheral library call to set Readout Protection on STM32F10x:

I call FLASH_ReadOutProtection(ENABLE)

I have put a flag into this function to verify that it's setting OB->RDP = 0x00

everything seems fine, except...

it doesn't set readout protection.  Even after a power cycle, when I call

FLASH_GetReadOutProtectionStatus()

I get a result 0

This is corroborated using STLink-V2

Any ideas?

#rdp #readout-protection
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Amel NASRI
ST Employee
Posted on November 10, 2014 at 17:36

Hi Henry,

Did you tried to use the ST-Link Utility?

This can help yo to confirm if issue is in hardware side or firmware one.

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Posted on November 10, 2014 at 18:07

Try doing it without the debugger attached, and pay attention to flags and status

void Flash_ReadOutProtection(int x) // 0=Status, 1=Lock, 2=Unlock - sourcer32@gmail.com
{
printf(''Flash_ReadOutProtection :

'');
if (FLASH_GetReadOutProtectionStatus())
printf(''Read Out Protected

'');
else
printf(''Read Out Un-Protected

'');
FLASH_Unlock();
FLASH_ClearFlag(FLASH_FLAG_BSY | FLASH_FLAG_EOP | FLASH_FLAG_PGERR | FLASH_FLAG_WRPRTERR);
if (x == 1)
{
printf(''Attempting to lock

'');
if (FLASH_GetReadOutProtectionStatus() != SET)
{
if (FLASH_ReadOutProtection(ENABLE) == FLASH_COMPLETE)
printf(''Read Out Passed

'');
else
printf(''Read Out Failed

'');
}
printf(''Cycle Power Now!

'');
Debug_Flush(); // Ensure telemetry clears threshold
while(1);
// NVIC_GenerateSystemReset();
}
else if (x == 2)
{
printf(''Attempting to unlock, Cycle Power Now!

'');
Debug_Flush();
FLASH_ReadOutProtection(DISABLE); // If it succeeds it nukes the part, not coming back here
}
}

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
hrobinson
Associate II
Posted on November 10, 2014 at 18:48

Hi,

thanks -

Mayla, yes I tested using STLink_V2, which confirmed it was a firmware problem.

Clive, yes I was looking at all the flags and status returned, all looked as I would expect; the ONLY things that were wrong were that FLASH_GetReadOutProtectionStatus() was reporting 0 (not protected) and this was confirmed using ST-Link (i.e. independent and reliable means).

I did try with the debugger disconnected, same result.

What I have now noticed though, looking at your code - was that I was missing ''FLASH_Unlock()''.

Looking at the code for FLASH_ReadOutProtection() it seemed as though it was setting keys to authorize access, but in fact it's only authorizing access to the Option bytes.  I needed FLASH_Unlock() to unlock the FPEC first!!!

So now it all works.

Thanks!