cancel
Showing results for 
Search instead for 
Did you mean: 

If I programmed a region of Flash protected by PCROP., how I can I modify the rest of the code, download and debug it with the STM32CubeIDE? In other words, is it possible to download code only in Bank1 and nothing in Bank2, hence keeping the PCROP region

JMene.1
Associate III
 
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Bubbles
ST Employee

Yes, it's possible. You mainly need to skip the mass erase and download only what was erased, for example one bank.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

JMene.1
Associate III

Thanks. But there is a way to do it easely with the cubeIDE or I need to change the makefile?