2021-10-20 5:03 AM
2021-10-20 5:29 AM
It depends on the RDP level whether you can remove it: level 1 is reversible, level 2 is a one-way street and not reversible.
For more details please read section Read protection (RDP) in the reference manual of your STM32.
Regards
/Peter
2021-10-20 5:51 AM
Level 1 it is, suggest me to resolve this issue
@Peter BENSCH ench
Even there is No info in datasheet
2021-10-20 5:59 AM
Right, the data sheet does not contain any information on this because it is not a device-specific question, but a family-specific one. As I have already written, the information can be found in the reference manual.
2021-10-20 6:23 AM
What mode of connectivity are you using?
Should be possible to walk the part out of RDP via the serial port and ROM based System Loader. With BOOT0=HIGH user code will not run, and not interfere with debug pins/connectivity.
You fail to mention which STM32, as I recall AN-3155 describes the loader commands.
Segger/J-Link used to have a specific STM32 tools to reset/recover the devices into a usable state.