cancel
Showing results for 
Search instead for 
Did you mean: 

Bootloader + Application Issue - Not working with Nucleo-wb55rg and STM32U585 discovery kit

rdund.11
Associate II

Hello,

I've two STM32 development kit and would like to implement and test the secure boot loader, however it's not working. There is NO serial print after programming boot loader G0_BL.bin load or Application G0_App4BL.bin. I read the location of 0x08000000 and 0x08008200, i see there exists code.

​The code i've referred is from the below video

Video reference: Security Part4 - STM32 security in practice - 10 Simple boot loader lab

The development kits i'm using are

  1. ​Nucleo-wb55rg
  2. STM32U585 discovery kit 

Can you please help me here what i'm missing.

Thanks & Regards

Rajesh

This discussion is locked. Please start a new topic to ask your question.
11 REPLIES 11
Hi Jocelyn,
Is the new STM32CubeU5 1.2.0 released?Can you please share the same.
Thanks & Regards
Raj

Hello @rdund.1​ ,

the new CubeU5 1.2.0 is now available here

I didn't check last week, maybe it arrived a bit late.

Best regards

Jocelyn