Writing multiple blocks to SD card fails
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-08-02 5:19 AM
Hello. I am developing application that involves writing multiple blocks (of 512 bytes) to SD card. It is a part of USB MSC application, multiblock operations are required for correct and fast functioning. A
BSP_SD_WriteBlocks() recommended routine hangs when writing several blocks. Reading multiple blocks performs OK, writing single block also is fine, but multiple blocks write transmission fails.
My code is simple:BSP_SD_WriteBlocks((uint32_t *)buf, blk_addr, blk_len, 1000);
uint32_t state1 = PERSONAL_SD_GetCardState();
uint32_t error1 = PERSONAL_SD_GetCardError() ;
//HANGS HERE while (BSP_SD_GetCardState() != SD_TRANSFER_OK) { }I have added two subroutines to stm32746g_discovery_sd.h to understand what is happening with card:
uint32_t
PERSONAL_SD_GetCardState
(void) { return ( (uint32_t)(HAL_SD_GetCardState(&uSdHandle) ) );}uint32_tPERSONAL_SD_GetCardError
(void) { return uSdHandle.ErrorCode;}During debug:
state1 gets assigned to 6 , which is 'Card is receiving operation information'. (I am expecting it to be 1, or card ready)
error1 gets assigned to 8 , which is 'Data timeout' (I am expecting it to be SDMMC_ERROR_NONE, or 0)
How can I overcome this issue and make sd card correctly accept several blocks in one operation?
#sdio #stm32f746-disco #sd-card- Labels:
-
SDIO-SDMMC
-
STM32F7 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2017-08-02 11:07 PM
Seems like I should construct my own subroutine that writes multiple blocks using a direct access to registers.
Does someone have an example of this code? Share it, please...
STM32F746NGH MCU's reference manual has quite vague instructions on how to do this (p. 1208) (CMD24, I need CMD25), and it covers only single block writing (which works OK with HAL code)
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-06-25 4:07 PM
Hello everybody,
I have some issue by using the read multiple block cmd, some data is corrupted.
T_U32 ReadBlock(T_U8* SrcData, T_U32 BlockAdd , T_U32 NumberOfBlocks )
{
HAL_DMA_Start_IT(hsd->hdmarx, (uint32_t)&hsd->Instance->FIFO, BlockAdd , (uint32_t)(BlockSize * NumberOfBlocks)/4);
if(this->SD_Card.CardType != CARD_SDHC_SDXC)
{ BlockAdd *= 512U; } SDIO_ConfigData()SDMMC_CmdBlockLength(registers, BLOCKSIZE);
BLOCKSIZE=512;
if(NumberOfBlocks > 1U)
{ StatusRead = SDMMC_CmdReadMultiBlock(registers, BlockAdd); } else { StatusRead = SDMMC_CmdReadSingleBlock(registers, BlockAdd); }It's necessary to send the
CmdBlockLength command after the SDMMC_CmdReadMultiBlock ,or it must change the BLOCKSIZE parameter to NumberOfBlocks * BlockSize within the CmdBlockLength.
thanks
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-06-25 6:09 PM
I note that the
ReadSingleBlock command is worked !!