cancel
Showing results for 
Search instead for 
Did you mean: 

With STM32F429I-DISCO Along side of ''IS42S16400J SDRAM'' Connecting another FMC Device?

bharadwajtke
Associate II
Posted on April 27, 2015 at 16:18

Dear All,

Is it Possible to Connect another FMC device along side of IS42S16400J in STM32F429I-DISCO

board, does the Address line and Data line causes any problem to the other FMC device from the onboard SD RAM(IS42S16400J )

Note: External device Voltage is same as the SDRAM Voltage level, Control lines are different for the External interfacing device,Except Data and the Address bus are shared Between SDRAM and the External FMC device.

Thanks for your valuable response, in advance.

#stm32f429i-disco-fmc-is42s16400j
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
ali rostami
Associate III

This is my question too. It seems that the answer is yes, as I took a look at the schematic of evaluation board.

But my question is, when we want to read data from nand flash should we disable sdram?

Is there any example of doing this?