cancel
Showing results for 
Search instead for 
Did you mean: 

WiFi VCOM Example Not Working

Drake Miller
Associate II
Posted on March 10, 2018 at 17:45

Hi, 

   I just purchased the following setup:

Computer: i7 / Windows 10

Nucleo: STM32F401

Expansion: IDW04A1

I have Trustudio as the compiler currently. Updated drivers to current.  

My problem is that when working the hands-on tutorial I can not get past the VCOM example.

I drop the Project.bin into the Nucleo board per the instructions open a terminal window and get only garbage output from the Wifi module. The blue LED2 is flashing and the others are solid (LED1 and LED4).  

I am stuck and not sure how to proceed if I can't get the module to work with this simple example. 

Thank you in advance for any insights here. 

Drake

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0