Why low the GPIO output speed?
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-12-14 1:47 PM
Dear ST Community,
The MCU type is: STM32F407VGT6
I try to write GPIOx->ODR register with DMA2. The trigger signal is TIM1 update event. I set the timer period frequency is 9Mhz and i measure 4.429Mhz on GPIO pin. Why?
here is my code:
#include "stm32f4xx.h"
uint8_t puffer[100];
int main(void)
{
SET_BIT(FLASH->ACR, FLASH_ACR_PRFTEN | FLASH_ACR_DCEN | FLASH_ACR_ICEN);
SET_BIT(DBGMCU->CR, DBGMCU_CR_DBG_SLEEP | DBGMCU_CR_DBG_STANDBY | DBGMCU_CR_DBG_STOP);
//HSE: 24Mhz
SET_BIT(RCC->CR, RCC_CR_HSEON);
while(!READ_BIT(RCC->CR, RCC_CR_HSERDY));
//PLL: 162Mhz
SET_BIT(RCC->PLLCFGR, RCC_PLLCFGR_PLLSRC);
MODIFY_REG(RCC->PLLCFGR, RCC_PLLCFGR_PLLM, 12 << RCC_PLLCFGR_PLLM_Pos);
MODIFY_REG(RCC->PLLCFGR, RCC_PLLCFGR_PLLN, 162 << RCC_PLLCFGR_PLLN_Pos);
MODIFY_REG(RCC->PLLCFGR, RCC_PLLCFGR_PLLP, 0 << RCC_PLLCFGR_PLLP_Pos);
SET_BIT(RCC->CR, RCC_CR_PLLON);
while(!READ_BIT(RCC->CR, RCC_CR_PLLRDY));
//FLASH
MODIFY_REG(FLASH->ACR, FLASH_ACR_LATENCY, 5 << FLASH_ACR_LATENCY_Pos);
//egyéb órajel osztók
MODIFY_REG(RCC->CFGR, RCC_CFGR_HPRE, 0 << RCC_CFGR_HPRE_Pos); //AHB /1
MODIFY_REG(RCC->CFGR, RCC_CFGR_PPRE1, 5 << RCC_CFGR_PPRE1_Pos); //APB1 /4
MODIFY_REG(RCC->CFGR, RCC_CFGR_PPRE2, 4 << RCC_CFGR_PPRE2_Pos); //APB2 /2
//switch to PLL
MODIFY_REG(RCC->CFGR, RCC_CFGR_SW, 2 << RCC_CFGR_SW_Pos);
//load buffer
for(uint8_t i=0;i<100;i +=2)
{
puffer[i] = 0;
puffer[i+1] = 255;
}
//TIM1 Ch1 9Mhz PWM -> PE9
SET_BIT(RCC->AHB1ENR, RCC_AHB1ENR_GPIOEEN);
MODIFY_REG(GPIOE->MODER, GPIO_MODER_MODE9, 2 << GPIO_MODER_MODE9_Pos); //AF
MODIFY_REG(GPIOE->AFR[1], GPIO_AFRH_AFRH1, 1 << GPIO_AFRH_AFSEL9_Pos);
MODIFY_REG(GPIOE->OSPEEDR, GPIO_OSPEEDER_OSPEEDR9, 3 << GPIO_OSPEEDR_OSPEED9_Pos); //Very high speed
SET_BIT(RCC->APB2ENR, RCC_APB2ENR_TIM1EN);
TIM1->ARR = 17; //162Mhz / 18 = 9Mhz
TIM1->CCR1 = 8; //50% PWM
/*TIM1->PSC = 2499;
TIM1->ARR = 64799;
TIM1->CCR1 = 32399; //1s*/
MODIFY_REG(TIM1->CCMR1, TIM_CCMR1_OC1M, 6 << TIM_CCMR1_OC1M_Pos);
SET_BIT(TIM1->CCER, TIM_CCER_CC1E);
SET_BIT(TIM1->BDTR, TIM_BDTR_MOE);
SET_BIT(TIM1->DIER, TIM_DIER_UDE); //Update DMA request enabled DMA2_Stream5 -> Channel6
//DMA2
SET_BIT(RCC->AHB1ENR, RCC_AHB1ENR_DMA2EN);
CLEAR_BIT(DMA2_Stream5->CR, DMA_SxCR_EN); //Stream 5 kikapcsolása TIM1_UP
while(READ_BIT(DMA2_Stream5->CR, DMA_SxCR_EN));
DMA2_Stream5->PAR = (uint32_t)&GPIOC->ODR;
DMA2_Stream5->M0AR = (uint32_t)&puffer[0];
DMA2_Stream5->NDTR = 100;
MODIFY_REG(DMA2_Stream5->CR, DMA_SxCR_CHSEL, 6 << DMA_SxCR_CHSEL_Pos); //Channel6
MODIFY_REG(DMA2_Stream5->CR, DMA_SxCR_PL, 3 << DMA_SxCR_PL_Pos); // Priority level: Very high
MODIFY_REG(DMA2_Stream5->CR, DMA_SxCR_DIR, 1 << DMA_SxCR_DIR_Pos); // Memory-to-peripheral
SET_BIT(DMA2_Stream5->CR, DMA_SxCR_MINC); // Memory address pointer is incremented after each data transfer (increment is done according to MSIZE)
//MODIFY_REG(DMA2_Stream5->CR, DMA_SxCR_PSIZE, 1 << DMA_SxCR_PSIZE_Pos); //Peripheral data size: Half-word (16-bit)
SET_BIT(RCC->AHB1ENR, RCC_AHB1ENR_GPIOCEN);
MODIFY_REG(GPIOC->MODER, GPIO_MODER_MODE0, 1 << GPIO_MODER_MODE0_Pos);
MODIFY_REG(GPIOC->OSPEEDR, GPIO_OSPEEDER_OSPEEDR0, 0 << GPIO_OSPEEDR_OSPEED0_Pos);
SET_BIT(DMA2_Stream5->CR, DMA_SxCR_EN);
SET_BIT(TIM1->CR1, TIM_CR1_CEN);
while (1)
{
/*SET_BIT(GPIOE->BSRR, 1 << 10);
SET_BIT(GPIOE->BSRR, 1 << 26);*/
/*SET_BIT(GPIOD->ODR, 1 << 0);
CLEAR_BIT(GPIOD->ODR, 1 << 0);*/
if(READ_BIT(DMA2->HISR, DMA_HISR_TCIF5))
{
SET_BIT(DMA2->HIFCR, DMA_HIFCR_CTCIF5 | DMA_HIFCR_CHTIF5);
DMA2_Stream5->NDTR = 100;
SET_BIT(DMA2_Stream5->CR, DMA_SxCR_EN);
}
}
}
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-12-14 2:03 PM
9MHz update, it means 111ns between the DMA events. One DMA event sets the pin, another - after 111ns - clears it, yet another - 222ns from the first - sets it again. That's s 222ns period, i.e. 4.5MHz frequency.
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2018-12-14 2:06 PM
You are right, I was wrong, I'm stupid :face_with_tears_of_joy:
Thank you :)