cancel
Showing results for 
Search instead for 
Did you mean: 

While Debugging STM32F303RC

Kapil Sharma
Associate II
Posted on February 13, 2018 at 10:40

  1. #@Hi everyone,

I am Kapil Sharma,

I have custom Board.When i am trying to debug code running  successfully and the Command log of Keil shows this..

* JLink Info: Found SW-DP with ID 0x2BA01477

* JLink Info: Found SW-DP with ID 0x2BA01477

* JLink Info: Scanning AP map to find all available APs

* JLink Info: AP[1]: Stopped AP scan as end of AP map has been reached

* JLink Info: AP[0]: AHB-AP (IDR: 0x24770011)

* JLink Info: Iterating through AP map to find AHB-AP to use

* JLink Info: AP[0]: Core found

* JLink Info: AP[0]: AHB-AP ROM base: 0xE00FF000

* JLink Info: CPUID register: 0x410FC241. Implementer code: 0x41 (ARM)

* JLink Info: Found Cortex-M4 r0p1, Little endian.

* JLink Info: FPUnit: 6 code (BP) slots and 2 literal slots

* JLink Info: CoreSight components:

* JLink Info: ROMTbl[0] @ E00FF000

* JLink Info: ROMTbl[0][0]: E000E000, CID: B105E00D, PID: 000BB00C SCS-M7

* JLink Info: ROMTbl[0][1]: E0001000, CID: B105E00D, PID: 003BB002 DWT

* JLink Info: ROMTbl[0][2]: E0002000, CID: B105E00D, PID: 002BB003 FPB

* JLink Info: ROMTbl[0][3]: E0000000, CID: B105E00D, PID: 003BB001 ITM

* JLink Info: ROMTbl[0][4]: E0040000, CID: B105900D, PID: 000BB9A1 TPIU

* JLink Info: ROMTbl[0][5]: E0041000, CID: B105900D, PID: 000BB925 ETM

ROMTableAddr = 0xE00FF000

* JLink Info: Reset: Halt core after reset via DEMCR.VC_CORERESET.

* JLink Info: Reset: Reset device via AIRCR.SYSRESETREQ.

can you provide me any solution for my problem?

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
AvaTar
Lead
Posted on February 13, 2018 at 11:00

What problem ?

I can't see any error message in the log.

And the question is 'assumed answered' anyway ...

Kapil Sharma
Associate II
Posted on February 13, 2018 at 11:05

While i am debugging the code the comment log shows below

* JLink Info: Reset: Halt core after reset via DEMCR.VC_CORERESET.

* JLink Info: Reset: Reset device via AIRCR.SYSRESETREQ.
Posted on February 13, 2018 at 12:21

And how do you come to think of this as an error ?

The debug adapter resets the core in order to invoke the reset vector/handler, and start the user application.