cancel
Showing results for 
Search instead for 
Did you mean: 

Which chip provide RX pin active level inversion

Jerry Lin
Associate II
Posted on January 31, 2018 at 08:12

I found that I can adjust UART RX pin active level inversion in CubeMX with STM32F303

but there is no such selection with STM32F405

I wonder which chip support that function

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
waclawek.jan
Super User
Posted on February 01, 2018 at 00:15

'F0, 'F3, 'F7, 'H7, 'L0, 'L4

JW

Posted on February 01, 2018 at 01:43

>>I wonder which chip support that function

If in doubt consider reviewing the Reference Manual, usually has such details.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..