2021-12-14 6:21 AM
2021-12-14 6:29 AM
It is located as comment (undefined) in system_stm32l4xx.c, which usually contains:
/*!< Uncomment the following line if you need to relocate the vector table
anywhere in Flash or Sram, else the vector table is kept at the automatic
remap of boot address selected */
/* #define USER_VECT_TAB_ADDRESS */Regards
/Peter
2021-12-14 6:29 AM
It is located as comment (undefined) in system_stm32l4xx.c, which usually contains:
/*!< Uncomment the following line if you need to relocate the vector table
anywhere in Flash or Sram, else the vector table is kept at the automatic
remap of boot address selected */
/* #define USER_VECT_TAB_ADDRESS */Regards
/Peter
2021-12-15 2:42 AM
Thanks @Peter BENSCH
2021-12-15 3:04 AM
If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.
/Peter