2026-01-30 1:33 AM
I work on an STM32F407G-DISC1 pedometer project, in which the program is supposed to use built-in lis3dsh accelerometer via SPI to detect and count steps and display the number of steps on the screen (ILI9341 SPI).
I have tested my screen code, and it works properly, so problem lies in how I use accelerometer or detect steps.
To detect steps, I read lis3dsh registers with 100HZ frequency by making a call to SPI from a 100HZ timer interrupt. These snippets are interrupt and timer configuration respectively.
void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef* htim)
{
if (htim->Instance == TIM2) {
if ((draw_ready == 1) && (accelerometer_ready == 1)) {
accelerometer_read_all_axes_dma(xyz_data, &hspi1);
}
}
//else if (htim->Instance == TIM3) {
// if (draw_ready == 1) {
//steps_count += 1;
//update_lcd_flag = 1;
// }
//}
}static void MX_TIM2_Init(void)
{
/* USER CODE BEGIN TIM2_Init 0 */
/* USER CODE END TIM2_Init 0 */
TIM_ClockConfigTypeDef sClockSourceConfig = {0};
TIM_MasterConfigTypeDef sMasterConfig = {0};
/* USER CODE BEGIN TIM2_Init 1 */
/* USER CODE END TIM2_Init 1 */
htim2.Instance = TIM2;
htim2.Init.Prescaler = 999;
htim2.Init.CounterMode = TIM_COUNTERMODE_UP;
htim2.Init.Period = 1679;
htim2.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
htim2.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
if (HAL_TIM_Base_Init(&htim2) != HAL_OK)
{
Error_Handler();
}
sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL;
if (HAL_TIM_ConfigClockSource(&htim2, &sClockSourceConfig) != HAL_OK)
{
Error_Handler();
}
sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;
sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
if (HAL_TIMEx_MasterConfigSynchronization(&htim2, &sMasterConfig) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN TIM2_Init 2 */
/* USER CODE END TIM2_Init 2 */
}The accelerometer is initialized at the start of the program using a function defined in accelerometer.c file. The following snippets are main and accelerometer functions respectively.
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration--------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* USER CODE BEGIN Init */
/* USER CODE END Init */
/* Configure the system clock */
SystemClock_Config();
/* USER CODE BEGIN SysInit */
/* USER CODE END SysInit */
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_DMA_Init();
MX_I2S3_Init();
MX_SPI1_Init();
MX_USB_HOST_Init();
MX_SPI2_Init();
MX_TIM2_Init();
MX_TIM3_Init();
/* USER CODE BEGIN 2 */
//timers
HAL_TIM_Base_Start_IT(&htim2);
HAL_TIM_Base_Start_IT(&htim3);
//Reset the screen
ILI9341_Init(&hspi2);
//screen experiment, delete later (black rectangle)
HAL_Delay(1000);
//Write_Rectangle(0, 50, 0, 50, 0, &hspi2); //good
//draw_digit(10, 10, 12, 8, 0, &hspi2); //good
//draw_number(UINT32_MAX, 12, &hspi2); //good
//Set everything for the accelometer
//fill buffer with 0s
for (int i = 0; i < ACC_BUF_SIZE; i++) {
acc_values_buf[i] = 0;
}
//receive and set accelerator sensitivity
accelerometer_init(&hspi1);
accelerometer_ready = 1;
//initial dma call (deprecated)
//HAL_SPI_TransmitReceive_DMA(&hspi1, xyz_addr, xyz_data, 6);
//default value
//clean_screen(0xFF, &hspi2);
//draw_number(steps_count, 12, &hspi2);
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
uint32_t steps_count_prev = -1;
clean_screen(0xFFFF, &hspi2);
draw_ready = 1;
while (1)
{
/* USER CODE END WHILE */
MX_USB_HOST_Process();
/* USER CODE BEGIN 3 */
//During each SPI clock cycle, full-duplex transmission of a single bit occurs.
//1 clock cycle is 168/32MHz = 5.25MHz
//meaning there are 5.25 * 10^6 bit, or 5.25 * 10^6/8 bytes = 656250 bytes
//or, all coordinates are received 109375 times.
if (update_lcd_flag == 1) {
Write_Rectangle(0, 30, 0, ILI9341_WIDTH - 1, 0xFFFF, &hspi2);
draw_number(steps_count, 12, &hspi2);
update_lcd_flag = 0;
}
steps_count_prev = steps_count;
}
/* USER CODE END 3 */
}
#include "accelerometer.h"
void accelerometer_read_all_axes_dma(uint8_t src[7], SPI_HandleTypeDef *hspi1) {
uint8_t tx[7] = {OUT_X_L | 0x80, 0, 0, 0, 0, 0, 0};
uint8_t rx[7];
HAL_GPIO_WritePin(ACC_GPIO_PORT, ACC_GPIO_PIN, GPIO_PIN_RESET);
HAL_SPI_TransmitReceive_DMA(hspi1, tx, src, 7);
HAL_GPIO_WritePin(ACC_GPIO_PORT, ACC_GPIO_PIN, GPIO_PIN_SET);
//memcpy(src, &rx[1], 6);
}
uint8_t accelerometer_read(uint8_t reg, SPI_HandleTypeDef *hspi1) {
//https://stackoverflow.com/questions/67922914/stm32-spi-communication-with-hal
HAL_GPIO_WritePin(ACC_GPIO_PORT, ACC_GPIO_PIN, GPIO_PIN_RESET);
uint8_t tx[2];
uint8_t rx[2];
tx[0] = reg | 0x80; // READ bit
tx[1] = 0x00; //the master transmits a dummy byte for the purpose of generating more clocks on which the slave can respond
HAL_SPI_TransmitReceive(hspi1, tx, rx, 2, 100); //send and receive 1 byte
HAL_GPIO_WritePin(ACC_GPIO_PORT, ACC_GPIO_PIN, GPIO_PIN_SET);
return rx[1];
}
void accelerometer_write(uint8_t reg, uint8_t val, SPI_HandleTypeDef *hspi1) {
HAL_GPIO_WritePin(ACC_GPIO_PORT, ACC_GPIO_PIN, GPIO_PIN_RESET);
uint8_t tx[2];
tx[0] = reg & 0x7F;
tx[1] = val;
HAL_SPI_Transmit(hspi1, tx, 2, 100);
HAL_GPIO_WritePin(ACC_GPIO_PORT, ACC_GPIO_PIN, GPIO_PIN_SET);
}
void accelerometer_init(SPI_HandleTypeDef *hspi1) {
//we don't need a queue
accelerometer_write(FIFO_CTRL, 0x00, hspi1);
//set sensitivity to 4
uint8_t ctrl_val;
ctrl_val = accelerometer_read(CTRL_REG5, hspi1);
ctrl_val = ctrl_val | 0x08; //set FSCALE0 so that sensitivity is +-4gg
uint8_t tx_buf[2];
tx_buf[0] = CTRL_REG5 & 0x7F; //register address
tx_buf[1] = ctrl_val; //data to write into it
accelerometer_write(CTRL_REG5, ctrl_val, hspi1);
//enable the device
uint8_t ctrl4_val = 0x7F;
accelerometer_write(CTRL_REG4, ctrl4_val, hspi1);
}The steps are detected in SPI1 callback. The following functions are SPI1 initialization and SPI1 RtRx callback respectively.
static void MX_SPI1_Init(void)
{
/* USER CODE BEGIN SPI1_Init 0 */
/* USER CODE END SPI1_Init 0 */
/* USER CODE BEGIN SPI1_Init 1 */
/* USER CODE END SPI1_Init 1 */
/* SPI1 parameter configuration*/
hspi1.Instance = SPI1;
hspi1.Init.Mode = SPI_MODE_MASTER;
hspi1.Init.Direction = SPI_DIRECTION_2LINES;
hspi1.Init.DataSize = SPI_DATASIZE_8BIT;
hspi1.Init.CLKPolarity = SPI_POLARITY_LOW;
hspi1.Init.CLKPhase = SPI_PHASE_1EDGE;
hspi1.Init.NSS = SPI_NSS_SOFT;
hspi1.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_32;
hspi1.Init.FirstBit = SPI_FIRSTBIT_MSB;
hspi1.Init.TIMode = SPI_TIMODE_DISABLE;
hspi1.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
hspi1.Init.CRCPolynomial = 10;
if (HAL_SPI_Init(&hspi1) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN SPI1_Init 2 */
/* USER CODE END SPI1_Init 2 */
}
//spi callback function
void HAL_SPI_TxRxCpltCallback(SPI_HandleTypeDef * hspi)
{
HAL_GPIO_WritePin(ACC_GPIO_PORT, ACC_GPIO_PIN, GPIO_PIN_SET);
if(hspi == &hspi1) {
//declare variables
int16_t x, y, z;
uint32_t mag;
uint32_t prev_index, prev_prev_index, prev_sample, prev_prev_sample;
prev_index = 0; prev_prev_index = 0; prev_sample = 0; prev_prev_sample = 0;
//calculate magnitude
x = (int16_t)((uint16_t)xyz_data[1] | ((uint16_t)xyz_data[2] << 8));
y = (int16_t)((uint16_t)xyz_data[3] | ((uint16_t)xyz_data[4] << 8));
z = (int16_t)((uint16_t)xyz_data[5] | ((uint16_t)xyz_data[6] << 8));
int32_t x32, y32, z32;
x32 = x; y32 = y; z32 = z;
mag = (uint32_t)(x32*x32 + y32*y32 + z32*z32); //auto-convert float to int //was sqrt
last_peak += 1; //when the last time there was a peak
value_period = 0;
prev_index = buf_index; //previous sample index
prev_prev_index = (prev_index == 0) ? (ACC_BUF_SIZE - 1) : (prev_index - 1); //(prev_index - 1) % ACC_BUF_SIZE; //pre-previous sample index
prev_sample = acc_values_buf[prev_index];
prev_prev_sample = acc_values_buf[prev_prev_index];
buf_index = (buf_index + 1) % ACC_BUF_SIZE; //update buf_index
acc_values_buf[buf_index] = mag; //add the sample
//make all checks
if ((last_peak < MAX_PEAK_DIFF && last_peak > MIN_PEAK_DIFF)
&& (prev_sample > prev_prev_sample)
&& (prev_sample > mag)
&& (prev_sample > PEAK_CUTOFF)) {
steps_count += 1; //uncomment later
update_lcd_flag = 1;
last_peak = 0;
}
else {
//update_lcd_flag = 0;
}
}
}In the TxRx callback function, I compare the previous sample (each sample is sum of squared x/y/z values) with the one before it and the current sample. If the previous sample is greater than either of its to neighbors, greater than a cutoff (which is supposed to be 0.35g), and it has been between 20 and 90 samples since the last sample corresponding all these conditions (this condition performs as a filter), it gets counted as a step.
The following snippets are constants and global variables used in the code above
#define MAX_PEAK_DIFF 90 //100 per second, so 90 to include slow walk
#define MIN_PEAK_DIFF 20 //100 per second, so 20 to include run
#define PEAK_CUTOFF 8220334 //0.35 g (32,767^2/(4^2)*(0.35^2))
#define ACC_BUF_SIZE 100 //1 second = 109375
uint32_t acc_values_buf[ACC_BUF_SIZE];
volatile uint8_t xyz_addr[6];
volatile uint8_t xyz_data[7];
uint32_t value_period = 0;
uint32_t buf_index = 0;
uint32_t last_peak = 0;
volatile uint32_t steps_count = 0;
volatile uint32_t update_lcd_flag = 1;
volatile uint32_t screen_dma_filled = 0;
volatile uint32_t bytes_remaining = 0;
extern volatile uint8_t dma_buf[PIXEL_BUFFER_SIZE];
uint32_t draw_ready = 0;
volatile int accelerometer_ready = 0;
#define FIFO_CTRL 0x2E
#define CTRL_REG4 0x20
#define ACC_GPIO_PORT GPIOE
#define ACC_GPIO_PIN GPIO_PIN_3
#define OUT_X_L 0x28
#define OUT_X_H 0x29
#define OUT_Y_L 0x2A
#define OUT_Y_H 0x2B
#define OUT_Z_L 0x2C
#define OUT_Z_H 0x2D
#define CTRL_REG5 0x24I think that the problem is either in step detection logic, or lis3dsh initialization, but I am not sure what the root of the problem is exactly.
2026-01-30 1:56 AM
I would recommend to review some publicly available (and working) pedometer projects, and how they assess accelerometer data to detect a "step".
> I compare the previous sample (each sample is sum of squared x/y/z values) with the one before it and the current sample. If the previous sample is greater than either of its to neighbors, greater than a cutoff (which is supposed to be 0.35g), and it has been between 20 and 90 samples since the last sample corresponding all these conditions (this condition performs as a filter), it gets counted as a step.
From first glance, I would think this is a bit too simple.
I would record a few samples with the board from actual steps, and review the value.
MEMS data are noisy to some extend, perhaps you need to apply some filtering.
> The accelerometer is initialized at the start of the program using a function defined in accelerometer.c file.
And I would highly recommend to download and read the datasheet of the LIS3DSH, and study the configuration section. A 100Hz SPI output rate does not imply a 100Hz sample rate.
> In the TxRx callback function, I ...
And I would avoid doing any evaluations in callback functions, which are interrupt context.
Better set a flag, and process the data in the main loop.
Not sure what the exact SPI interrupt context is, but evaluating every single sample on its own seems inefficient.
No need to update a pedometer every few milliseconds, so two or three screen updates (and thus data evaluation cycles) are more than enough.
2026-01-30 3:25 AM - edited 2026-01-30 3:40 AM
SPI itself does not have 100Hz sampling rate (it is 168 Mhz/32, since it is the faster value that is less than 10MhZ I could get), there is a 100Hz timer that causes reads of samples.
I will probably move the evaluations to the main loop, thank you for the advice.
2026-01-30 3:28 AM
Start with checking the data you get from the accelerometer in static state. Check 1g for each axis. Does that data make sense that you get?
Then continue checking the data you get from the moving sensor.
2026-01-30 3:37 AM
How do I know the values when the board is not connected to the PC?
2026-01-30 5:45 AM
What do you mean? How do you test the pedometer?
For checking 1g on all axes you can stay connected to the PC, just turn the board in each direction.
DC-coupled accelerometers are so easy to calibrate on earth... :D
And for the pedometer: your algorithm should show steps even when moving up and down rhythmically, so shake your board...