cancel
Showing results for 
Search instead for 
Did you mean: 

What is the expected future production run for the STM32 Nucleo-144 reference board? And while at that, for the MCU as wel, the STM32F746ZGT. Thank you advance.

PGild.1
Associate III

Is the MCU "not for new" designs?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Welcome, @PGild.1​, to the community!

The NUCLEO boards are an important part of the development support and will therefore not disappear from the market any time soon.

However, in contrast to the rolling commitment of the STM32, there is no product longevity of 10 years for the NUCLEO, which is also not necessary, since they do not represent a final product.

Yes, you can definitely use the STM32F746ZGT for new designs.

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Peter BENSCH
ST Employee

Welcome, @PGild.1​, to the community!

The NUCLEO boards are an important part of the development support and will therefore not disappear from the market any time soon.

However, in contrast to the rolling commitment of the STM32, there is no product longevity of 10 years for the NUCLEO, which is also not necessary, since they do not represent a final product.

Yes, you can definitely use the STM32F746ZGT for new designs.

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
PGild.1
Associate III

Thank you very much Peter for the speedy answer!

It indeed answers my question.

Have a nice day.

Pieter