2020-04-26 12:07 PM
Hello ,
I would like to get some examples for WFE based sleep . In stm32cube examples, i see that most of them are like WFI based examples. Request someone to help me with this information. Thanks in advance.
Regards,
Vinoth
Solved! Go to Solution.
2020-05-03 6:39 AM
After searching for while i attempted myself with the understanding from the datasheet.
It works. Hope it helps someone in need. Thanks to @TDK .
Code snippet for SEVONPEND = 1 as below
int main(void)
{
/* Add your application code here */
__IO uint32_t tmpreg;
/* Enable clock for toggle LED */
SET_BIT(RCC->AHB1ENR, RCC_AHB1ENR_GPIOIEN);
tmpreg = READ_BIT(RCC->AHB1ENR, RCC_AHB1ENR_GPIOIEN);
/* Enable clock for switch input (EXTI) */
SET_BIT(RCC->AHB1ENR, RCC_AHB1ENR_GPIOCEN);
tmpreg = READ_BIT(RCC->AHB1ENR, RCC_AHB1ENR_GPIOCEN);
/* Enable clock for SYSCFG that connects switch to EXTI */
SET_BIT(RCC->APB2ENR, RCC_APB2ENR_SYSCFGEN);
tmpreg = READ_BIT(RCC->APB2ENR, RCC_APB2ENR_SYSCFGEN);
/* Configure toggle LED */
GPIOI->MODER |= GPIO_MODER_MODER15_0;
GPIOI->PUPDR |= GPIO_PUPDR_PUPDR15_0;
GPIOI->OSPEEDR |= GPIO_OSPEEDR_OSPEEDR15;
GPIOI->BSRR= GPIO_BSRR_BS15; // Reset
/* Configure switch input */
GPIOC->PUPDR = 0;
GPIOC->MODER = 0;
SYSCFG->EXTICR[3] = 0x20;
EXTI->IMR = 0x2000;
EXTI->EMR = 0;
EXTI->RTSR = 0x2000;
SET_BIT(SCB->SCR, ((uint32_t)SCB_SCR_SEVONPEND_Msk));
/* Infinite loop */
while (1)
{
/* Set SLEEPDEEP bit of Cortex System Control Register */
SCB->SCR |= SCB_SCR_SLEEPDEEP_Msk;
/* Ensure that all instructions done before entering SLEEP mode */
__DSB();
__ISB();
/* Request Wait For Event */
__SEV();
__WFE();
__WFE();
/* Reset SLEEPDEEP bit of Cortex System Control Register */
SCB->SCR &= (uint32_t)~((uint32_t)SCB_SCR_SLEEPDEEP_Msk);
/* Clear the flag responding to the event */
EXTI->PR = 0x2000;
while (EXTI->PR != 0);
/* Clear the pending flag responding to the event in NVIC */
NVIC_ClearPendingIRQ(EXTI15_10_IRQn);
ToggleLed();
}
}Code snippet for SEVONPEND = 0 as below
int main(void)
{
/* Add your application code here */
__IO uint32_t tmpreg;
/* Enable clock for toggle LED */
SET_BIT(RCC->AHB1ENR, RCC_AHB1ENR_GPIOIEN);
tmpreg = READ_BIT(RCC->AHB1ENR, RCC_AHB1ENR_GPIOIEN);
/* Enable clock for switch input (EXTI) */
SET_BIT(RCC->AHB1ENR, RCC_AHB1ENR_GPIOCEN);
tmpreg = READ_BIT(RCC->AHB1ENR, RCC_AHB1ENR_GPIOCEN);
/* Enable clock for SYSCFG that connects switch to EXTI */
SET_BIT(RCC->APB2ENR, RCC_APB2ENR_SYSCFGEN);
tmpreg = READ_BIT(RCC->APB2ENR, RCC_APB2ENR_SYSCFGEN);
/* Configure toggle LED */
GPIOI->MODER |= GPIO_MODER_MODER15_0;
GPIOI->PUPDR |= GPIO_PUPDR_PUPDR15_0;
GPIOI->OSPEEDR |= GPIO_OSPEEDR_OSPEEDR15;
GPIOI->BSRR= GPIO_BSRR_BS15; // Reset
/* Configure switch input */
GPIOC->PUPDR = 0;
GPIOC->MODER = 0;
SYSCFG->EXTICR[3] = 0x20;
EXTI->IMR = 0;
EXTI->EMR = 0x2000;
EXTI->RTSR = 0x2000;
/* Infinite loop */
while (1)
{
/* Set SLEEPDEEP bit of Cortex System Control Register */
SCB->SCR |= SCB_SCR_SLEEPDEEP_Msk;
/* Ensure that all instructions done before entering SLEEP mode */
__DSB();
__ISB();
/* Request Wait For Event */
__SEV();
__WFE();
__WFE();
/* Reset SLEEPDEEP bit of Cortex System Control Register */
SCB->SCR &= (uint32_t)~((uint32_t)SCB_SCR_SLEEPDEEP_Msk);
ToggleLed();
}
}
2020-04-26 12:53 PM
> WFE examples required for stm32 family?
Might want to narrow down STM32 family a bit. There are a lot of products out there.
Doesn't seem to be many CubeMX examples that use WFE. But here is one:
When I want examples, sometimes I use the raw GitHub search to find where things are used. A lot of hits are from the definition file, but some are in project usage:
https://github.com/search?q=PWR_SLEEPENTRY_WFE+filename%3A*.c+language%3AC+language%3AC&type=Code
2020-05-03 6:39 AM
After searching for while i attempted myself with the understanding from the datasheet.
It works. Hope it helps someone in need. Thanks to @TDK .
Code snippet for SEVONPEND = 1 as below
int main(void)
{
/* Add your application code here */
__IO uint32_t tmpreg;
/* Enable clock for toggle LED */
SET_BIT(RCC->AHB1ENR, RCC_AHB1ENR_GPIOIEN);
tmpreg = READ_BIT(RCC->AHB1ENR, RCC_AHB1ENR_GPIOIEN);
/* Enable clock for switch input (EXTI) */
SET_BIT(RCC->AHB1ENR, RCC_AHB1ENR_GPIOCEN);
tmpreg = READ_BIT(RCC->AHB1ENR, RCC_AHB1ENR_GPIOCEN);
/* Enable clock for SYSCFG that connects switch to EXTI */
SET_BIT(RCC->APB2ENR, RCC_APB2ENR_SYSCFGEN);
tmpreg = READ_BIT(RCC->APB2ENR, RCC_APB2ENR_SYSCFGEN);
/* Configure toggle LED */
GPIOI->MODER |= GPIO_MODER_MODER15_0;
GPIOI->PUPDR |= GPIO_PUPDR_PUPDR15_0;
GPIOI->OSPEEDR |= GPIO_OSPEEDR_OSPEEDR15;
GPIOI->BSRR= GPIO_BSRR_BS15; // Reset
/* Configure switch input */
GPIOC->PUPDR = 0;
GPIOC->MODER = 0;
SYSCFG->EXTICR[3] = 0x20;
EXTI->IMR = 0x2000;
EXTI->EMR = 0;
EXTI->RTSR = 0x2000;
SET_BIT(SCB->SCR, ((uint32_t)SCB_SCR_SEVONPEND_Msk));
/* Infinite loop */
while (1)
{
/* Set SLEEPDEEP bit of Cortex System Control Register */
SCB->SCR |= SCB_SCR_SLEEPDEEP_Msk;
/* Ensure that all instructions done before entering SLEEP mode */
__DSB();
__ISB();
/* Request Wait For Event */
__SEV();
__WFE();
__WFE();
/* Reset SLEEPDEEP bit of Cortex System Control Register */
SCB->SCR &= (uint32_t)~((uint32_t)SCB_SCR_SLEEPDEEP_Msk);
/* Clear the flag responding to the event */
EXTI->PR = 0x2000;
while (EXTI->PR != 0);
/* Clear the pending flag responding to the event in NVIC */
NVIC_ClearPendingIRQ(EXTI15_10_IRQn);
ToggleLed();
}
}Code snippet for SEVONPEND = 0 as below
int main(void)
{
/* Add your application code here */
__IO uint32_t tmpreg;
/* Enable clock for toggle LED */
SET_BIT(RCC->AHB1ENR, RCC_AHB1ENR_GPIOIEN);
tmpreg = READ_BIT(RCC->AHB1ENR, RCC_AHB1ENR_GPIOIEN);
/* Enable clock for switch input (EXTI) */
SET_BIT(RCC->AHB1ENR, RCC_AHB1ENR_GPIOCEN);
tmpreg = READ_BIT(RCC->AHB1ENR, RCC_AHB1ENR_GPIOCEN);
/* Enable clock for SYSCFG that connects switch to EXTI */
SET_BIT(RCC->APB2ENR, RCC_APB2ENR_SYSCFGEN);
tmpreg = READ_BIT(RCC->APB2ENR, RCC_APB2ENR_SYSCFGEN);
/* Configure toggle LED */
GPIOI->MODER |= GPIO_MODER_MODER15_0;
GPIOI->PUPDR |= GPIO_PUPDR_PUPDR15_0;
GPIOI->OSPEEDR |= GPIO_OSPEEDR_OSPEEDR15;
GPIOI->BSRR= GPIO_BSRR_BS15; // Reset
/* Configure switch input */
GPIOC->PUPDR = 0;
GPIOC->MODER = 0;
SYSCFG->EXTICR[3] = 0x20;
EXTI->IMR = 0;
EXTI->EMR = 0x2000;
EXTI->RTSR = 0x2000;
/* Infinite loop */
while (1)
{
/* Set SLEEPDEEP bit of Cortex System Control Register */
SCB->SCR |= SCB_SCR_SLEEPDEEP_Msk;
/* Ensure that all instructions done before entering SLEEP mode */
__DSB();
__ISB();
/* Request Wait For Event */
__SEV();
__WFE();
__WFE();
/* Reset SLEEPDEEP bit of Cortex System Control Register */
SCB->SCR &= (uint32_t)~((uint32_t)SCB_SCR_SLEEPDEEP_Msk);
ToggleLed();
}
}