cancel
Showing results for 
Search instead for 
Did you mean: 

Virtual COM Port ?

antonius
Senior
Posted on February 19, 2014 at 01:58

Guys,

I have installed STM Virtual COM Port on my computer,

But everytime I connect the board via USB cable, window says ''USB device is not recognized''

What shall I do to fix it ?

Thanks
This discussion is locked. Please start a new topic to ask your question.
15 REPLIES 15
Posted on February 21, 2014 at 03:27

The .DFU file is a specially packaged binary image, typically built from one or more .HEX or .BIN files using ST's DFU Manager tool.

The release notes suggest there are .HEX files, so use those.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
antonius
Senior
Posted on February 23, 2014 at 09:14

I put BOOT0 = 1 and uploaded Virtual COMport software with Jlink,

it didn't give me any responses, isn't my USB working ? or like you said, flawed ?

thanks

chen
Associate II
Posted on February 27, 2014 at 11:09

''I put BOOT0 = 1 and uploaded Virtual COMport software with Jlink,''

That does not sound right. With Boot0 set, DFU should be used to download.

''it didn't give me any responses, isn't my USB working ? or like you said, flawed ?''

I think we cannot tell since the download was not by DFU.

Does your downloaded program have any way to show it is running (eg flashing LED)?

apbqdo
Associate II
Posted on February 28, 2014 at 10:04

Rick, I have some problems with the VCP too. When you installed the driver, have you had a new device in Device Manager? (Without connecting the board.) As I understand it, the device should appear anyway, but I do not have any... Or they appear only when you connect the board?

chen
Associate II
Posted on February 28, 2014 at 10:09

Hi

''As I understand it, the device should appear anyway, but I do not have any... Or they appear only when you connect the board?''

It should only appear when the board is connected.

apbqdo
Associate II
Posted on February 28, 2014 at 10:24

Chen Chung, thank you, it makes it clearer.

Denis.