cancel
Showing results for 
Search instead for 
Did you mean: 

Virtual COM port in NUCLEO-F767ZI. Code 43. Samples and examples.

KKubr
Associate

Hello!

I bought a NUKLEO-F767ZI. I want to program a virtual COM port in CubeMX and Keil uVision5, but device's manager in my WINDOWS10 says "The Windows system stopped this device because it reported a problem." (Code 43) The request for the descriptor failed USB devices. "

But the built-in ST-LINK/V2-1 works well.

I tried many methods to fix this error, but nothing helps me.

Tell me please, where i can find Samples and Exaples for NUKLEO-F767ZI to program VCP?

Thanks!

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3

The should be assorted examples under the CubeF7 code trees, unpack and review. CubeMX should have unpacked in the repository. ​

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
KKubr
Associate

Thank you!

Tell me please, which folder is the repository?

James Murray
Senior

It depends where you unpacked it!

Search for something like:

STM32Cube_FW_F7_V1.12.0

and then see the Projects under that and find the most applicable directory.

James