2023-05-14 4:29 AM
I'm using a VS Code extension that most probably uses `vcpkg`. After installing this extension, each time I run VS Code I get the following error:
> Using vcpkg executable at "c:\Users\Luka\.vscode\extensions\ms-vscode.vscode-embedded-tools-0.7.0-win32-x64\assets\platform\win32-x64\vcpkg.exe".
> Using VCPKG_ROOT at "c:\Users\Luka\AppData\Roaming\Code\User\globalStorage\ms-vscode.vscode-embedded-tools\vcpkg\root".
> Activating environment at "c:\Repository\Code\STM32Cube\TestSTM32vscode\vcpkg-configuration.json".
> Version of vcpkg used to create VCPKG_ROOT: "2023-03-14-105f7f7e8a5ea10dfac9874ff9d1a6bacba5f454".
> Running vcpkg with arguments ["version"].
vcpkg package management program version 2023-03-14-105f7f7e8a5ea10dfac9874ff9d1a6bacba5f454
See LICENSE.txt for license information.
> Bundled version of vcpkg: "2023-03-14-105f7f7e8a5ea10dfac9874ff9d1a6bacba5f454".
> Running vcpkg with arguments ["activate","--project","c:\\Repository\\Code\\STM32Cube\\TestSTM32vscode","--json","C:\\Users\\Luka\\AppData\\Local\\Temp\\0b0bfd2e9086e9804700cf10fe331514"].
warning: vcpkg-artifacts is experimental and may change at any time.
Downloading vcpkg-artifacts bundle 2023-03-14...
Downloading github.com/microsoft/vcpkg-tool/releases/download/2023-03-14/vcpkg-ce.tgz
node:internal/modules/cjs/loader:1078
throw err;
^
Error: Cannot find module 'C:\Users\Luka\AppData\Local\vcpkg\artifacts-2023-03-14\node_modules\'
at Module._resolveFilename (node:internal/modules/cjs/loader:1075:15)
at Module._load (node:internal/modules/cjs/loader:920:27)
at Function.executeUserEntryPoint [as runMain] (node:internal/modules/run_main:81:12)
at node:internal/main/run_main_module:23:47 {
code: 'MODULE_NOT_FOUND',
requireStack: []
}
Node.js v18.16.0
> Failed with exit code "1".
> Failed to activate environment at "c:\Repository\Code\STM32Cube\TestSTM32vscode\vcpkg-configuration.json".I have checked the files it cannot find and found out that the `artifacts-2023-03-14` is empty. I have tried several possible solution to this problem on Stack Overflow but didn't manage to change anything.
Possible solutions on SO: https //stackoverflow.com/questions/53545800/internal-modules-cjs-loader-js582-throw-err/54964538#54964538
Any idea or hint to possible solution is very much appreciated!
2023-05-30 11:52 PM
I just have the same problem and solved by extracting the vcpkg-ce.tgz file manually.
2023-05-31 5:04 AM
@CsBe Could you please share a few additional details? I have tried to resolve the issue based on your comment, but I couldn't. I tried to put the contents of the zip file I can download via the link mentioned in the vcpkg-configuration.json file and put it manually into the vcpkg\artifacts-2023-03-14 folder. However, when I try to again run the project import tool, I get the same error, and the artifact folder is empty again (seems to get overwritten with an empty folder).
2023-08-28 5:47 PM
Uninstall and fresh install your VS code extensions. Most commonly, the CMake extension. That should solve your issue.