cancel
Showing results for 
Search instead for 
Did you mean: 

various defines stop working from includes

Jerry Hancock
Associate II

OK, I'm going crazy.

stm32f4xx_hal_def.h is included in just about every file. Defined in this header is Hal_StatusTypeDef - Not found when compiled. I made no changes that could have impacted this. Prior to Hal_StatusTypeDef not being found, I had others that were not found. Even when I moved the define right in front of the lines of code where used! At first I thought it had something to do with an include loop, but I can't find it. I've tried cleaning, etc.

Any ideas? This all started with one project but I've had others go off the rails like this as well.

Thanks

Jerry

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
waclawek.jan
Super User

You mean HAL_StatusTypeDef? C is case sensitive. Copy/paste is a good friend but a bad enemy.

JW

Jerry Hancock
Associate II

it's not that, I might have typed it in wrongn here.

I found something last night, or this morning around 2am, about the sequence of includes. Something might have changed in the latest version or version -1. When I reloaded sw4stm last night, it must have picked up the new version.

The thread I found over at Openstm32 was called "include madness" and it describes my problem exactly. It has to do with including stm32f4_hal.h from main.h because it is was already started to be included from stm32f469i_discovery.h or somewhere else in the chain. So the person proposed a change to include files.

The other issue is all the stdint.h entries have now disappeared in the same mess. I should have left well enough alone.

Jerry

Probably need to invest in a better class of tools.

Check the Include Paths passed to the compiler, including the order of them

Check the defines called out in stm32f4xx_hal_conf.h

Check the defines passed to the compiler, USE_HAL_DRIVER, etc

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..