cancel
Showing results for 
Search instead for 
Did you mean: 

using the DMA controller as a camera interface

hurwitze
Associate II
Posted on June 19, 2008 at 18:31

using the DMA controller as a camera interface

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
hurwitze
Associate II
Posted on May 17, 2011 at 12:37

Hi I looked at the application note an2548, which describes how to use the DMA controller as a camera interface. The example tells you to connect the camera data inputs (8 bit wide) to Port PD. However, I cannot connect to this port because it is already in use as the connection to external SRAM. In addition I would like to use the DMA controller in the following manner:

The DMA source should be Port PC (since I have that one available)

The DMA destination should be the external SRAM through the FSMC.

Is this possible? Can I connect the camera output data lines to port PC?

Thanks.

hurwitze
Associate II
Posted on May 17, 2011 at 12:37

by the way, I am using the stm32f103z.

16-32micros
Associate III
Posted on May 17, 2011 at 12:37

Hi hurwitze,

Yes you can ! have a look on example ''FSMC'' in ''DMA'' examples subfolers from the STM32 FW library : it uses two DMA1 channels to transfer a word data buffer from embedded FLASH to external memory through FSMC and from this external memory to embedded RAM. Yo can just tailor and combine with AN2548 example. Let's us know if you make it working ?

Cheers,

STOne-32. :o (Release Your Creativity)

hurwitze
Associate II
Posted on May 17, 2011 at 12:37

Thank you. I will try it out and let you know. Right now I am designing the hardware, so that hopefully the software will be easier :)