cancel
Showing results for 
Search instead for 
Did you mean: 

Using ST Link on Discovery board as standalone ST Link

dbmiller5
Associate
Posted on February 02, 2013 at 09:12

I have

http://www.sainsmart.com/sainsmart-stm32f103rbt6-arm-cortex-m3-mini-development-board-code-jlink-v8-adapter.html

 (board only), and I need

JTAG debugger to program it.  Is it possible to use my F1 discovery as a JTAG debugger for the purpose of programming?  I am totally new to STM32, but I am excited to learn.  

Thanks, 

Dave
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Posted on February 02, 2013 at 11:15

You should be able use a VL-Discovery to program it via the SWD connections. You'd need to remove the internal jumpered connections, and then wire up the SWDIO (JTMS), SWCLK (JTCK), and GND to the associated pins on the 20-pin JTAG header.

In an ideal world you'd probably want NRST too.

The SWD header does not provide for full JTAG functionality.
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
ken239955
Associate II
Posted on February 02, 2013 at 21:24

That is exactly how I am using my STM32F0DISCOVERY as clive describes it. You only need two wires plus ground.