cancel
Showing results for 
Search instead for 
Did you mean: 

Using an oscillator for LSE in battery mode?

Lars Beiderbecke
Senior III

Suppose I use an oscillator instead of the suggested resonator for LSE. Will that even work, i.e., will the internal RTC continue to function when in battery mode? I assume that I'd have to power both oszillator and STM32 (using Vbat)?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

Which STM32?

Most probably yes. Don't forget that RCC_BDCR.LSEBYP has to be set. There are mixed reports on whether RCC_BDCR.LSERDY is usable for that case; but that's not fatal.

JW

View solution in original post

2 REPLIES 2

Which STM32?

Most probably yes. Don't forget that RCC_BDCR.LSEBYP has to be set. There are mixed reports on whether RCC_BDCR.LSERDY is usable for that case; but that's not fatal.

JW

Lars Beiderbecke
Senior III

Thanks, I think I will give it a try, but maybe on an old board I have.