2010-02-10 01:16 AM
UsbHidDemonstrator error LNK2001
2011-05-17 04:39 AM
All it is ok ! I have reinstall the HidDemonstrator and I have correct 5 error on the sources code and it works !
Many error of variable declaration on the source code (fixed) An one error when the function ''ON_WM_NCHITTEST()'' are called on ''IconeButton.cpp'' (Don't fixed) : error C2440: 'static_cast' :impossible to convert
'UINT (__thiscall CIconButton::* )(CPoint)' en 'LRESULT (__thiscall CWnd::* )(CPoint)' c:\program files\stmicroelectronics\software\usb hid demonstrator\src\iconbutton.cpp 56 UsbHidDemonstrator So if you have a solution... Mickael.