2012-01-03 12:29 AM
Hi everybody,
i work with the evalboard STM3220G with the USB example from the USB host-device lib. I try to write additional data in the create/existing file, but I'm not successful. Can anyone say me, what i must chance to solve that problem?2012-01-06 6:59 AM
Folks I dont know if anyone else spotted this but
if you compare the file usbh_msc_fatfs.* in the STM32F2XX examples and STM32F4XX code its different by this in DRESULT disk_write () DRESULT disk_read () stm32f2xx status = USBH_MSC_Read10(&USB_OTG_Core, buff, sector, 512); status = USBH_MSC_Write10(&USB_OTG_Core,(BYTE*)buff, sector, 512); stm32f4xx status = USBH_MSC_Read10(&USB_OTG_Core, buff, sector, 512*count); status = USBH_MSC_Write10(&USB_OTG_Core,(BYTE*)buff, sector, 512*count); are you trying to manipulate lots of data ? the stm32F4xx code was in the stm32f4 STM32F4XXX\stm32f4discovery_fw\STM32F4-Discovery_FW_V1.1.0\Libraries where as stm32f2 code is the USB examples Dan2012-01-28 2:37 PM
I wish I had seen your post before I spent a few hours chasing down this problem! I only found this post once I was about to post my own bug report.
The F4 version appears to be the correct one. You have to put that multiply by ''count'' in there, or reads and writes will not do more than 512 bytes, despite how many sectors were specified. I was reading a file 4K at a time and was only getting holes in the middle of each block where no data was read.I haven't tested the write case yet, but the F4 version of the code seems to work fine for reads.