cancel
Showing results for 
Search instead for 
Did you mean: 

USART3 nucleo STM32F767ZI virtual com port

JVele.1
Associate

I have some problems to see in the serial port the message of my nucleo board, for this board I read that for USART 3 Virtual COM SB4 and SB7 most be off, and SB5 and SB6 on, for the st/link serial but nothing happens. I debug the code and all is working correctly but in the terminal theres nothing. I install st/link utility, st/virtual com port but nothing

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
DNusz.1
Associate

i know that feel bro

Karl Yamashita
Principal

Unless you have something connected to the Morpho connector then SB4 and SB7 doesn't need to be unsoldered. Out of the box the VCP should work. So it would come down to you not sending data correctly or the peripheral was not set up correctly. Post your IOC file and code.

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.
CAN Jammer an open source CAN bus hacking tool
CANableV3 Open Source