cancel
Showing results for 
Search instead for 
Did you mean: 

USART3 Clock setting is not working on STM32F334.

Honggi Choe
Associate
Posted on July 20, 2017 at 04:18

Hi Experts,

I'm a newbie to STM32F334 MCU. I need help on setting USART3 clock.

Two USARTS are used on the board. USART1 is used for PC communication. USART3 is used for BLE device communication internally.

PC communication was not working at first, characters were broken. USART1 was operating on default clock - PCLK - 36MHz. Changed USART1 clock to 8MHz - HSI through below API and it was working.

    /* Configure the HSI as USART1 clock */

    RCC_USARTCLKConfig(RCC_USART1CLK_HSI);

    /* Enable USART1 clocks */

    RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART1, ENABLE);

8.4.13 Clock configuration register 3 (RCC_CFGR3)

Address: 0x30

Reset value: 0x0000 0000

Bits 19:18 USART3SW[1:0]: USART3 clock source selection

This bit is set and cleared by software to select the USART3 clock source.

00: PCLK selected as USART3 clock source (default)

01: System clock (SYSCLK) selected as USART3 clock

10: LSE clock selected as USART3 clock

11: HSI clock selected as USART3 clock

Bits 1:0 USART1SW[1:0]: USART1 clock source selection

This bit is set and cleared by software to select the USART1 clock source.

00: PCLK selected as USART1 clock source (default)

01: System clock (SYSCLK) selected as USART1 clock

10: LSE clock selected as USART1 clock

11: HSI clock selected as USART1 clock

Now similarly USART3 is not working with default clock -36MHz PCLK to BLE device.

I am trying to change USART3 clock to 8MHz HSI clock through below API.

    /* Configure the HSI as USART3 clock */

    RCC_USARTCLKConfig(RCC_USART3CLK_HSI);

    /* Enable USART3 clocks */

    RCC_APB1PeriphClockCmd(RCC_APB1Periph_USART3, ENABLE);

But strangely USART3SW cannot be altered to 3 from 0. I tried to change USART3SW through JTAG but it was not changed.

Please help me to find out why USART3SW is not changed.

Thanks a lot for your help in advance.

BR,

Honggi

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Zhi Gu
Associate
Posted on July 26, 2017 at 05:58

Hi

I have a similar issue, and I tried to modified the 'USART3SW' of 'RCC->CFGR3' by Keil debug mode, but it doesn't work.