cancel
Showing results for 
Search instead for 
Did you mean: 

USART missed rx interrupt

Adalgiso
Associate II
Posted on July 04, 2013 at 14:37

Hi,

I have an STM3220g-sk/iar demo kit.

I try to configure the STM32F2 device to receive data with UART interrupt.

I have the following code

int main()

{

  /* Reset all the ports to default values */

  GPIO_DeInit(GPIOA);

  GPIO_DeInit(GPIOB);

  GPIO_DeInit(GPIOC);

  GPIO_DeInit(GPIOD);

  GPIO_DeInit(GPIOE);

  GPIO_DeInit(GPIOF);

  GPIO_DeInit(GPIOG);

  uart1_init();            

  while(1)

  {

    /* wait */    

  }

}

/*------------------------------------------------------------------------------

 * DESCRIPTION: intialize USART1  for serial communication

 *----------------------------------------------------------------------------*/

void uart1_init (void)

{

  GPIO_InitTypeDef GPIO_InitStructure;

  USART_InitTypeDef USART_InitStructure;  

  // Enable UART clock 

  RCC_APB2PeriphClockCmd(RCC_APB2Periph_USART6 , ENABLE); 

  

  // Enable GPIOA Clock

  RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC , ENABLE); 

  RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOG , ENABLE); 

  

   // Connect PA9 to USARTx_Tx

  GPIO_PinAFConfig(GPIOC, GPIO_PinSource6, GPIO_AF_USART6);

  

  // Connect PA10 to USARTx_Rx

  GPIO_PinAFConfig(GPIOG, GPIO_PinSource9, GPIO_AF_USART6);

  

  // Configure USART Tx as alternate function

  GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;

  GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP;

  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;

  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6;

  GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;

  GPIO_Init(GPIOC, &GPIO_InitStructure);

  // Configure USART Rx as alternate function

  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;

  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_9;

  GPIO_Init(GPIOG, &GPIO_InitStructure);

  /* UART0 configuration -----------------------------------------------------*/

  /* UART0 configured as follow:

  - Word Length = 8 Bits

  - Two Stop Bit

  - No parity

  - BaudRate = 115200 baud

  - Hardware flow control disabled 

  - Receive and transmit enabled

  */

  USART_InitStructure.USART_BaudRate = 115200;

  USART_InitStructure.USART_WordLength = USART_WordLength_8b;

  USART_InitStructure.USART_StopBits = USART_StopBits_1;

  USART_InitStructure.USART_Parity = USART_Parity_No;

  USART_InitStructure.USART_HardwareFlowControl =     USART_HardwareFlowControl_None;

  USART_InitStructure.USART_Mode = USART_Mode_Rx | USART_Mode_Tx;

 

  USART_Init(USART6, &USART_InitStructure);

  

  USART_ITConfig(USART6, USART_IT_RXNE, ENABLE);

  NVIC_InitTypeDef NVIC_InitStructure;

  // * Enable the USART Interrupt * /

  NVIC_InitStructure.NVIC_IRQChannel = USART6_IRQn;

  NVIC_InitStructure.NVIC_IRQChannelSubPriority = 1;

  NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority = 0;

  NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;

  NVIC_Init(&NVIC_InitStructure);  

 

  /* Enable UART0 */

  USART_Cmd(USART6, ENABLE);

}

void USART6_IRQHandler(void)

{

  u8 c;

  u8 info = 0;

  static u32 temp=0;

  static u32 int_count =0;

  static u32 rx_int_count =0;

  

  int_count++;

  if ( USART_GetITStatus ( USART6, USART_IT_ORE ) )

    {

        USART_ReceiveData(USART6);

    }

  /* TX INTERUPT IS TRIGGERED */

  /*

  if(USART_GetITStatus(RS422_HW.USART, USART_IT_TXE) != RESET)

  {

    info++;

    if(tx_cnt)                                           // if still some bytes to be sent, go on to the next one.  

    {

      tx_cnt--;                                                     // one byte has been sent              

      USART_SendData(USART6, (u16)tx_buf[tx_buf_index++]);

    }

    else                                       // Otherwise wait a bit before closing the TX slave port

    {

      RS422_sending_over = true;  

      USART_ITConfig(USART6, USART_IT_TXE, DISABLE);

      it_counter_rs422++;

    }

    

    led_control(LED_BUS_GREEN,2,0,1);                             // Blinks the BUS LED 10ms 

    led_control(LED_BUS_RED,2,0,1);                               // Blinks the BUS LED 10ms 

    

  }*/

  /* RX INTERUPT IS TRIGGERED */

  if(USART_GetITStatus(USART6, USART_IT_RXNE) != RESET)

  {  

    info++;

    {

      rx_int_count++;

      temp++;

      c = (u8)USART_ReceiveData(USART6) & (u8)(0xFF);    

    }

  }

  

  if (info ==0)

  {

        c = (u8)USART_ReceiveData(USART6) & (u8)(0xFF); 

        /* (uint16_t)(USARTx->DR & (uint16_t)0x01FF);

    ITStatus stat = USART_GetITStatus(RS422_HW.USART, USART_IT_TC);

    stat = USART_GetITStatus(RS422_HW.USART, USART_IT_PE);

    stat = USART_GetITStatus(RS422_HW.USART, USART_IT_TXE);

    stat = USART_GetITStatus(RS422_HW.USART, USART_IT_TC);

    stat = USART_GetITStatus(RS422_HW.USART, USART_IT_RXNE);

    stat = USART_GetITStatus(RS422_HW.USART, USART_IT_TC);

    stat = USART_GetITStatus(RS422_HW.USART, USART_IT_ORE_RX);

    stat = USART_GetITStatus(RS422_HW.USART, USART_IT_IDLE);

    stat = USART_GetITStatus(RS422_HW.USART, USART_IT_LBD);

    stat = USART_GetITStatus(RS422_HW.USART, USART_IT_CTS);

    stat = USART_GetITStatus(RS422_HW.USART, USART_IT_ERR);

    stat = USART_GetITStatus(RS422_HW.USART, USART_IT_ORE_ER);

    stat = USART_GetITStatus(RS422_HW.USART, USART_IT_NE);

    stat = USART_GetITStatus(RS422_HW.USART, USART_IT_FE);

    stat = USART_GetITStatus(RS422_HW.USART, USART_IT_TXE);

    stat = USART_GetITStatus(RS422_HW.USART, USART_IT_RXNE);

    stat = USART_GetITStatus(RS422_HW.USART, USART_IT_TXE);

        */

  } 

}

The main issue is that when sending byte 1 by 1, it works but when I sent more bytes with no pause in between each byte, I get only 1 time in the interrupt.

If instead of using the interrupt I do poll the  USART_FLAG_RXNE flag, it works fine and I do not miss any byte.

Any idea?

#stm32f2-usart #interrupt #lost
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0