USART interrupt problem
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2011-08-18 10:52 PM
Hi Guys, I'm working on Usart programming in IAR environment. But I got a problem. The USART interrupt handler seemed not to be called. Here's my code:
void initUART2()
{
USART_InitTypeDef uart2Init;
USART_ClockInitTypeDef uart2ClockInit;
GPIO_InitTypeDef gpioA;
NVIC_InitTypeDef NVIC_InitStructure;
RCC_APB1PeriphClockCmd( RCC_APB1Periph_USART2, ENABLE );
RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA, ENABLE);
///////////SetUart2 GPIO
gpioA.GPIO_Pin=GPIO_Pin_2;
gpioA.GPIO_Speed=GPIO_Speed_50MHz;
gpioA.GPIO_Mode=GPIO_Mode_AF_PP;
GPIO_Init( GPIOA, &gpioA);
gpioA.GPIO_Pin = GPIO_Pin_3;
gpioA.GPIO_Mode = GPIO_Mode_IN_FLOATING;
GPIO_Init(GPIOA, &gpioA);
//////////////////////////InitUART
uart2Init.USART_BaudRate=9600;
uart2Init.USART_WordLength=USART_WordLength_8b;
uart2Init.USART_StopBits=USART_StopBits_1;
uart2Init.USART_Parity=USART_Parity_No;
uart2Init.USART_Mode=USART_Mode_Rx|USART_Mode_Tx;
uart2Init.USART_HardwareFlowControl=USART_HardwareFlowControl_None;
USART_Init(USART2,&uart2Init);
////////////////////////////InitUARTClock
uart2ClockInit.USART_Clock=0;//USART_Clock_Enable;
uart2ClockInit.USART_CPOL=0;//USART_CPOL_Low;
uart2ClockInit.USART_CPHA=0;//USART_CPHA_1Edge;
uart2ClockInit.USART_LastBit=0;//USART_LastBit_Disable;
USART_ClockInit(USART2,&uart2ClockInit);
/////////////////InterruptConfig
NVIC_InitStructure.NVIC_IRQChannel = USART2_IRQn;
NVIC_InitStructure.NVIC_IRQChannelPreemptionPriority =3;
NVIC_InitStructure.NVIC_IRQChannelSubPriority = 0;
NVIC_InitStructure.NVIC_IRQChannelCmd = ENABLE;
NVIC_Init( &NVIC_InitStructure );
USART_ITConfig( USART2, USART_IT_RXNE, ENABLE );
USART_ClearFlag(USART1,USART_FLAG_TC);
//////////////////Enable UART
USART_Cmd(USART2,ENABLE);
}
//////////////////////////
///////////////////////////////////
void USART2_IRQHandler(void)
{
if(USART_GetITStatus(USART2, USART_IT_RXNE) != RESET)
{
/* Read one byte from the receive data register */
RxBuffer2[RxCounter++] = USART_ReceiveData(USART2);
/* Clear the USART2 Receive interrupt */
USART_ClearITPendingBit(USART2, USART_IT_RXNE);
if(RxCounter == 100)
{
/* Disable the USART2 Receive interrupt */
USART_ITConfig(USART2, USART_IT_RXNE, DISABLE);
}
}
}
Are there problems in my source code? Plz, help me! Thanks!
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2011-08-19 6:08 AM
Well, I'd suggest you initialize the NVIC immediately after the RCC.
With the NVIC, be sure to set the vector table for your environment and the priority group. Don't bother with the USART clock initialization, if you must use it, put it before the USART init, but for regular serial comms the default peripheral settings are fine. Interrupts do work properly on all three USARTs. Confirm you are actually receiving data properly without interrupts.Up vote any posts that you find helpful, it shows what's working..