cancel
Showing results for 
Search instead for 
Did you mean: 

Uploading to target devkit error. I have 2 x STM32F769 Discovery Kit. in 1 kit it's always running without any problem. in another kit most of the time I'm getting this error while uploading.

RMuru.1
Associate II

Run Target

  Generate

    Done

  Generate Assets

    make -f simulator/gcc/Makefile assets -j8

    Reading ./application.config

    Done

  Post Generate

    touchgfx update_project --project-file=simulator/msvs/Application.vcxproj

    Done

  Post Generate Target

    touchgfx update_project --project-file=../STM32F769I_DISCO.ioc --platform=m7

    Done

  Compile

    make -f ../gcc/Makefile -j8

    Reading TouchGFX/application.config

    Linking TouchGFX/build/bin/target.elf

    Producing additional output formats...

     target.hex  - Combined internal+external hex

     intflash.elf - Internal flash, elf debug

     intflash.hex - Internal flash, hex

     extflash.bin - External flash, binary

    Done

  Flash

    make -f ../gcc/Makefile flash

    Reading TouchGFX/application.config

    Linking TouchGFX/build/bin/target.elf

    Producing additional output formats...

     target.hex  - Combined internal+external hex

     intflash.elf - Internal flash, elf debug

     intflash.hex - Internal flash, hex

     extflash.bin - External flash, binary

       -------------------------------------------------------------------

                STM32CubeProgrammer v2.7.0          

       -------------------------------------------------------------------

     

    ST-LINK SN : 0671FF544856846687084030

    ST-LINK FW : V2J37M27

    Board    : 32F769IDISCOVERY

    Voltage   : 3.23V

    SWD freq  : 4000 KHz

    Connect mode: Normal

    Reset mode : Software reset

    Device ID  : 0x451

    Revision ID : Rev Z

    Device name : STM32F76x/STM32F77x

    Flash size : 2 MBytes

    Device type : MCU

    Device CPU : Cortex-M7

     

     

     

    Memory Programming ...

    Opening and parsing file: target.hex

     File     : target.hex

     Size     : 3180204 Bytes

     Address    : 0x08000000 

     

     

    Erasing memory corresponding to segment 0:

    Erasing internal memory sectors [0 4]

    Erasing memory corresponding to segment 1:

    Erasing external memory sectors [0 44]

    Download in Progress:

    ±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±±± 0%

    ÛÛÛÛÛÛÛÛ 16%ÛÛÛ 23%ÛÛÛÛÛÛÛÛÛ 40%ÛÛÛÛÛÛÛÛ 56%ÛÛÛÛÛÛÛÛ 72%ÛÛÛÛÛÛÛÛ 88%Error: Unable to get core ID

     

     

    Error: failed to download Segment[1]

    Error: failed to download the File

     

     

    Error: Unable to reset MCU!

    d:/Srushty/Smart_Watch/STMProject/Tranquility_STM_project/gcc/include/flash_sections_int_ext.mk:2: recipe for target '_extflash_' failed

    make[1]: *** [_extflash_] Error 1

    ../gcc/Makefile:53: recipe for target 'flash' failed

    make: *** [flash] Error 2

    Failed

  Failed

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0