cancel
Showing results for 
Search instead for 
Did you mean: 

UNIQUE ID

Farhad13651
Associate II

Hi

Is the UNIQUE ID of the STM32H562RIT6 microcontroller, which consists of 96 bits, entirely variable, or does it include fixed bits as well? Which bits are fixed?

1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

The Unique ID is so called because it is actually exactly unique - across all STM32 that have ever been produced (if they support this feature). It does not contain any fixed bits; they vary from chip to chip. The respective reference manual contains a description of the structure.

Does this answer your question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Peter BENSCH
ST Employee

The Unique ID is so called because it is actually exactly unique - across all STM32 that have ever been produced (if they support this feature). It does not contain any fixed bits; they vary from chip to chip. The respective reference manual contains a description of the structure.

Does this answer your question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.