cancel
Showing results for 
Search instead for 
Did you mean: 

unable to get output in 3.5"tft spi display having ili9488 driver

charu_mathi
Visitor

I am currently working on a project using the STM32F401RE Nucleo board interfaced with a 3.5-inch TFT SPI display (ILI9488 driver). I am facing an issue where the display does not show any output, even though the backlight turns on and the code uploads successfully without errors.

I have already checked the SPI connections, power supply, and display initialization code, but the screen still  remains blank. I would like to kindly request your guidance or any reference materials/libraries that can help me correctly configure and test the display with STM32CubeIDE.

If possible, I would appreciate help with:

  • Correct SPI configuration for ILI9488

  • Required GPIO pin mapping (DC, RESET, CS, etc.)

  • A working example code or initialization sequence

  • Any known issues or recommended libraries for STM32F4 + ILI9488

Your support will greatly help me continue my project. Thank you

0 REPLIES 0