cancel
Showing results for 
Search instead for 
Did you mean: 

UM1734 Error - USB Device - CDC

bobseabrook9
Associate II
Posted on May 03, 2016 at 11:50

pdf:      UM1734

rev:      3

page:     52/59

Section: 6.5.6

step:      4

bug:       text wrongly reads: CDC control requests should be handled by the function Controllability().

fix:        state the name of a function or callback or template that actually exists in the CDC Standalone example or the CubeMx v4.14+ generated code, or correctly identify as the relevant IRQ handler if that is whats is meant.

#m.b.a
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Amel NASRI
ST Employee
Posted on May 03, 2016 at 16:55

Hi seabrook.bob,

Please note that your feedback is reported internally to be taken into account in coming version of UM1734.

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.