Skip to main content
abeba.1
Associate III
November 2, 2022
Question

udp_client on stm32 h753 nuclio board

  • November 2, 2022
  • 0 replies
  • 532 views

hii

i have stm32 nucleo-h753 board and i finally managed to set the project in order to work with the ethernet port .

i can ping the board successfully , so my next step is to send udp message from the board to my pc .

i use herculis as my udp server .

i run the project and in the herculis terminal i don't see a message received from the client (my stm board )

during the running i can ping the board successfully .

i uploaded the main function , my main goal is to send a single message to the hurculis terminal .

i be glad for help please :)

This topic has been closed for replies.