UART/USART IT Handler Has No Callback
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2017-12-02 2:08 PM
Posted on December 02, 2017 at 23:08
In stm32L4xx_hal_uart.c and usart.c for the HAL Driver version 1.10.0, a call to HAL_UART_IRQHandler returns back to the caller if no errors instead of HAL_UART_RxCpltCallback. This is contrary to the descriptive comments in the beginning of the driver source that says a callback is used for non-blocking mode. Non-blocking in DMA mode returns to a callback.
Unlike the HAL COMM_IT example I am using a 1 word buffer.
I have not checked other driver versions.
Cheers, Hal
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2017-12-03 12:26 PM
Posted on December 03, 2017 at 21:26
I have found that there is not allways a call to the callback in the ISR routine. You have to add them yourself.