cancel
Showing results for 
Search instead for 
Did you mean: 

uart printf echo back not working without a printf in USART2_IRQHandler (using HAL)

ckim
Associate II
Posted on December 17, 2015 at 09:23

Hi,

I'm using uVision5 on windows7 to build and flash download but doing the experiment on Linux machine.(because UART COM port doesn't work on my win7 PC. I think this is a driver problem.). I've slightly modified the Uart_printf project so that the program prints something and receives commands from the console and prints it back. Below is the main() program.

============ in main.c ===============

char Rx_indx, Rx_data[2], Rx_Buffer[100], Transfer_cplt;

UART_HandleTypeDef UartHandle;

char buffer[100];

int len;

void HAL_UART_RxCpltCallback(UART_HandleTypeDef *huart)

{

        uint8_t i;

        if (huart->Instance == USART2) // current UART

        {

                if (Rx_indx==0) {for (i=0;i<100;i++) Rx_Buffer[i] = 0; }

                if (Rx_data[0] != 13) // if not enter

                {

                        Rx_Buffer[Rx_indx++] = Rx_data[0]; // add data to Rx_Buffer

                }

                else {

                        Rx_indx = 0;

                        Transfer_cplt=1; // transfer complete, data is ready to be read

                }

                HAL_UART_Receive_IT(&UartHandle, (uint8_t *)Rx_data, 1); // reactivate

        }

}

int main(void)

{

        HAL_Init();

        SystemClock_Config();

        -- set USART2

                ...

        HAL_UART_Receive_IT(&UartHandle, (uint8_t *)Rx_data, 1); 

        printf(''hello, World!\r\n'');

        while (1) {

                if (Transfer_cplt)

                {

                        sprintf(buffer, ''%s\r\n'', Rx_Buffer);

                        len = strlen(buffer);

                        HAL_UART_Transmit(&UartHandle, (uint8_t *)buffer, len, 1000);

                        Transfer_cplt = 0;

                }

        }

        while (1)

        {

        }

}

======= in stm32f4xx_it.c ================

void SysTick_Handler(void)

{

        HAL_IncTick();

        HAL_SYSTICK_IRQHandler();

}

void USART2_IRQHandler(void)

{

printf(''USART2_IRQHandler called\n\r'');    <==== !!! not work without this line.

        HAL_UART_IRQHandler(&UartHandle);

}

========== end of code =========

Below is the execution result when I have the ''USART2_IRQHandler called'' print in the USART2_IRQHandler(void) function.

hello, World!

USART2_IRQHandler called

USART2_IRQHandler called

USART2_IRQHandler called

USART2_IRQHandler called

USART2_IRQHandler called

abcd

USART2_IRQHandler called

USART2_IRQHandler called

USART2_IRQHandler called

USART2_IRQHandler called

USART2_IRQHandler called

efgh

USART2_IRQHandler called

USART2_IRQHandler called

USART2_IRQHandler called

USART2_IRQHandler called

USART2_IRQHandler called

xyzg

hello, World!

USART2_IRQHandler called

USART2_IRQHandler called

USART2_IRQHandler called

USART2_IRQHandler called

USART2_IRQHandler called

abcd

But if I remove the print (''USART2_IRQHandler called'') the print-back is not shown. What is wrong with the code?

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0