cancel
Showing results for 
Search instead for 
Did you mean: 

two can bus with stm32f407 at the same time

omid hope
Associate
Posted on December 15, 2017 at 11:32

hi i want to have two can bus with stm32f407 can1 and can2. can1 for node 1 to 5 and can2 for node 6 to 10. but i receive data just in one bus at the same time. how should i config can1 & 2 in this case?

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0