2008-11-17 04:39 AM
True performance of STM32?
#stm322011-05-17 03:19 AM
@slawcus:
Quote:
On 21-10-2008 at 13:27, Anonymous wrote: Where did you get this ''MISP test''?2011-05-17 03:19 AM
To jrnore,
Did you try with ARM or IAR compiler? May be you will get 1.25 DMIPS/Mhz2011-05-17 03:19 AM
Hi all,
In 2010,a New STM32F2xx will be available with zero-wait program execution up to 120MHz :http://www.st.com/stonline/stappl/cms/press/news/year2010/t24htm
For unique performance benefiting from the 90nm process and the ART memory accelerator have been verified according to CoreMark™ tests created by the Embedded Microprocessor Benchmark Consortium. CoreMark results verify the STM32 executes 8% faster than Cortex-M competitors at 100MHz clock speed. The performance advantage is greater still at 120MHz. CoreMark analysis also confirms dynamic power consumption of only 188µA/MHz (98µA/CoreMark). This is equivalent to drawing 5mA at 120MHz (executing from Flash memory, with ART accelerator enabled and all peripherals off). Continue releasing your Creativity2011-05-17 03:19 AM
In worst cases, the critical code can run in RAM with 0 waitstate.