cancel
Showing results for 
Search instead for 
Did you mean: 

True performance of STM32?

lspr35
Associate II
Posted on November 17, 2008 at 13:39

True performance of STM32?

#stm32
53 REPLIES 53
lspr35
Associate II
Posted on May 17, 2011 at 12:19

@slawcus:

Quote:

On 21-10-2008 at 13:27, Anonymous wrote:

Where did you get this ''MISP test''?

jilisegiar
Associate II
Posted on May 17, 2011 at 12:19

To jrnore,

Did you try with ARM or IAR compiler?

May be you will get 1.25 DMIPS/Mhz

Posted on May 17, 2011 at 12:19

Hi all,

In 2010,a New STM32F2xx will be available with zero-wait program execution up to 120MHz :

http://www.st.com/stonline/stappl/cms/press/news/year2010/t24htm

For unique performance benefiting from the 90nm process and the ART memory accelerator have been verified according to CoreMark™ tests created by the Embedded Microprocessor Benchmark Consortium. CoreMark results verify the STM32 executes 8% faster than Cortex-M competitors at 100MHz clock speed. The performance advantage is greater still at 120MHz. CoreMark analysis also confirms dynamic power consumption of only 188µA/MHz (98µA/CoreMark). This is equivalent to drawing 5mA at 120MHz (executing from Flash memory, with ART accelerator enabled and all peripherals off).

Continue releasing your Creativity

0690X0000060MkwQAE.gif

STOne-

benoit239955_stm1_st
Associate II
Posted on May 17, 2011 at 12:19

In worst cases, the critical code can run in RAM with 0 waitstate.