cancel
Showing results for 
Search instead for 
Did you mean: 

trouble writing firmware

nswami11
Associate
Posted on January 04, 2011 at 11:05

trouble writing firmware

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
nswami11
Associate
Posted on May 17, 2011 at 14:20

Hi,

I got past the previous trouble. I can now write the firmware STM3210E-EVAL_Demo_V2.0.dfu that I downloaded from st.com to the Internal Flash through dfusudemo.exe.

I am now trying to build firmware and write to Internal Flash. I'm using Ride IDE and the sources and project file that came with um059.zip. I convert the hex file to dfu file using DFU File Mgr and try to download the dfu file to Internal Flash. This doesn't work. It fails the Verify cycle.

Is this supposed to work? I am wondering if there is a problem with the memory map.

Thanks. I would appreciate any help,

Swami