cancel
Showing results for 
Search instead for 
Did you mean: 

transmission and reception problems with stm32f103c8 with nrf24 library

Cnnon.1
Associate

hello, i am developing my project in a stm32f103c8 (bluepill) with Keil and CubeMX, i want to use a nrf24l01 transmitter and for this i looked for a tutorial which is exactly what i want to do. the problem is that when i do it i notice that the radio transceiver does not transmit or receive, i have seen on the internet that some people have problems with this card that i am using, just me this is failing me using this library. I leave a link to a video that shows the same steps that I made in addition to the library. precisely the function nrf24_write is the one that is not working. I hope you can help me because I've been trying to understand why it does not work for several days.

link video:

https://www.youtube.com/watch?v=O2dg2Eo7vo8

link library:

https://github.com/MYaqoobEmbedded/STM32-Tutorials/tree/master/Tutorial%2024%20-%20NRF24L01%20Radio%20Transceiver

main code:

/* Includes ------------------------------------------------------------------*/
#include "main.h"
 
/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#include "MY_NRF24.h"
#include "stdio.h"
/* USER CODE END Includes */
 
/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */
 
/* USER CODE END PTD */
 
/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
/* USER CODE END PD */
 
/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */
 
/* USER CODE END PM */
 
/* Private variables ---------------------------------------------------------*/
SPI_HandleTypeDef hspi1;
 
UART_HandleTypeDef huart1;
 
/* USER CODE BEGIN PV */
 
/* USER CODE END PV */
 
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_SPI1_Init(void);
static void MX_USART1_UART_Init(void);
/* USER CODE BEGIN PFP */
 
/* USER CODE END PFP */
 
/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */
uint64_t TxpipeAddrs = 0x324e6f6465;
char myTxData[32]; //= "Hello World!";
char AckPayload[32];
/* USER CODE END 0 */
 
/**
  * @brief  The application entry point.
  * @retval int
  */
int main(void)
{
  /* USER CODE BEGIN 1 */
	myTxData[0]= 0;
  /* USER CODE END 1 */
 
  /* MCU Configuration--------------------------------------------------------*/
 
  /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
  HAL_Init();
 
  /* USER CODE BEGIN Init */
 
  /* USER CODE END Init */
 
  /* Configure the system clock */
  SystemClock_Config();
 
  /* USER CODE BEGIN SysInit */
 
  /* USER CODE END SysInit */
 
  /* Initialize all configured peripherals */
  MX_GPIO_Init();
  MX_SPI1_Init();
  MX_USART1_UART_Init();
  /* USER CODE BEGIN 2 */
	NRF24_begin(GPIOB, GPIO_PIN_8, GPIO_PIN_9, hspi1);
	nrf24_DebugUART_Init(huart1);
	
	
	
	//**** TRANSMIT - ACK ****//
	
	NRF24_setPALevel(RF_PWR_HIGH);
	NRF24_openWritingPipe(TxpipeAddrs);
 
	NRF24_setAutoAck(true);
	NRF24_setChannel(52);
	NRF24_setPayloadSize(32);
	NRF24_setDataRate(RF24_2MBPS);
	
	NRF24_enableDynamicPayloads();
	NRF24_enableAckPayload();
	NRF24_stopListening();
	HAL_Delay(1000);
	printRadioSettings();
  /* USER CODE END 2 */
 
  /* Infinite loop */
  /* USER CODE BEGIN WHILE */
  while (1)
  {
    /* USER CODE END WHILE */
		if(NRF24_write(myTxData, 32))
		{
			NRF24_read(AckPayload, 32);
			HAL_UART_Transmit(&huart1, (uint8_t *)"Transmitted Successfully\r\n", strlen("Transmitted Successfully\r\n"), 10);
			
			char myDataack[80];
			sprintf(myDataack, "AckPayload:  %s \r\n", AckPayload);
			HAL_UART_Transmit(&huart1, (uint8_t *)myDataack, strlen(myDataack), 10);
		}else{
					HAL_UART_Transmit(&huart1, (uint8_t *)"Transmitted Failed\r\n", strlen("Transmitted Failed\r\n"), 10);}
		myTxData[0]= myTxData[0] + 1;
		HAL_Delay(1000);
    /* USER CODE BEGIN 3 */
  }
  /* USER CODE END 3 */
}

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0