cancel
Showing results for 
Search instead for 
Did you mean: 

TM32-Discovery power on don't work

johnnymanke
Associate
Posted on July 08, 2012 at 02:03

Hello, I bought a STM32-Discovery, but when I turn on, the power led blink, and then the LED goes off. The PC dont detect a new hardware..

I measure the voltage in the TP1 is 0,85V. I think the board has a short but yet I dont know locate. I think if I remove the D1 BAT60JFILM, I measure 5 VCC from usb.

Somebody already had a problem equal?

Regards
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0