cancel
Showing results for 
Search instead for 
Did you mean: 

TIMx_CH1_ETR vs TIMx_CH1

moez0102
Associate II
Posted on July 12, 2018 at 14:55

Could you explain me the difference between TIMx_CH1_ETR and TIMx_CH1, please?

In deed, I would like to replace STM32L071 with STM32F091 (PA0 - pin n°14).

In general, I would like to connect an external clock to a timer pin. My goal is to use the timer alone when the processor in Idle mode to save power. So, could I use TIMx_CH1_ETR or TIMx_CH1 or both are allowed, please?

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
waclawek.jan
Super User
Posted on July 12, 2018 at 16:09

TIMx_CH1_ETR is a - somewhat confusing - way to tell, that this pin is connected internally to *both* the CH1 and the ETR nodes of the TIMx module.

In other words, as long as you don't use any of the ETR functions, you can use TIMx_CH1_ETR in exactly the same way as you use TIMx_CH1.

JW

Posted on July 13, 2018 at 09:24

Thanks,

However, when we use 

TIMx_ETR and when we use 

TIMx_CH1 in general, please?