cancel
Showing results for 
Search instead for 
Did you mean: 

TIM8 Toggle STM32F4

pedro
Associate II
Posted on June 26, 2015 at 12:32

Hi,

I'm trying to toggle some pins when timer 8 overflows. The problem I get is that I don´t see the pins toogle but I can see the timer counting on the debugger, so I think I might be missing some mistereous configuration on the GPIO. I'm using all 4 channels just for testing and I put a pulse value of half the timer period for testing aswell. The code I have so far:

void TIM8_Init(void){
TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;
TIM_OCInitTypeDef TIM_OCInitStructure;
GPIO_InitTypeDef GPIO_InitStructure;
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC, ENABLE);
RCC_APB2PeriphClockCmd(RCC_APB2Periph_TIM8 ,ENABLE);
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_6 | GPIO_Pin_7 | GPIO_Pin_8 | GPIO_Pin_9;
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_Speed = GPIO_High_Speed;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL;
GPIO_Init(GPIOC,&GPIO_InitStructure);
GPIO_PinAFConfig(GPIOC, GPIO_PinSource6 ,GPIO_AF_TIM8);
GPIO_PinAFConfig(GPIOC, GPIO_PinSource7 ,GPIO_AF_TIM8);
GPIO_PinAFConfig(GPIOC, GPIO_PinSource8 ,GPIO_AF_TIM8);
GPIO_PinAFConfig(GPIOC, GPIO_PinSource9 ,GPIO_AF_TIM8);
TIM_TimeBaseStructure.TIM_Period = 100; 
TIM_TimeBaseStructure.TIM_Prescaler = 0; 
TIM_TimeBaseStructure.TIM_ClockDivision = 0;
TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;
TIM_TimeBaseInit(TIM8, &TIM_TimeBaseStructure);
//Channel 1
TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_Toggle;
TIM_OCInitStructure.TIM_OutputState = TIM_OutputState_Enable;
TIM_OCInitStructure.TIM_OutputNState = TIM_OutputNState_Disable;
TIM_OCInitStructure.TIM_Pulse = 50;
TIM_OCInitStructure.TIM_OCPolarity = TIM_OCPolarity_High;
TIM_OCInitStructure.TIM_OCNPolarity = TIM_OCPolarity_High;
TIM_OCInitStructure.TIM_OCIdleState = TIM_OCIdleState_Reset;
TIM_OCInitStructure.TIM_OCNIdleState = TIM_OCNIdleState_Reset;
TIM_OC1Init(TIM8, &TIM_OCInitStructure);
TIM_OC2Init(TIM8, &TIM_OCInitStructure);
TIM_OC3Init(TIM8, &TIM_OCInitStructure);
TIM_OC4Init(TIM8, &TIM_OCInitStructure);
//TIM_DMACmd(TIM8, TIM_DMA_Update, ENABLE ); /* Enable TIM8_Updates DMA Requests */
//SET COUNTER
TIM8->CR1 = 0x1; 
}

Thanks :)
This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
kai_mauer
Associate
Posted on June 26, 2015 at 15:36

You write:
 

GPIO_Init(GPIOC,&GPIO_InitStructure);
GPIO_PinAFConfig(GPIOC, GPIO_PinSource6 ,GPIO_AF_TIM8);
GPIO_PinAFConfig(GPIOC, GPIO_PinSource7 ,GPIO_AF_TIM8);
GPIO_PinAFConfig(GPIOC, GPIO_PinSource8 ,GPIO_AF_TIM8);
GPIO_PinAFConfig(GPIOC, GPIO_PinSource9 ,GPIO_AF_TIM8);
 This itches me a little. Wrong order?
 First I would config the pins, then do GPIO_Init().
 I use HAL, so I explicitly cannot say whether the order is right or wrong. The HAL function set all regs at once...
 Have you looked in the GPIO AF reg with the debugger? 

Posted on June 26, 2015 at 15:43

Not sure the pin ordering matters, provided the GPIO clock is enabled, it's pins/mux are configurable.

  /* TIM8 (special) enable pins */

  TIM_CtrlPWMOutputs(TIM8, ENABLE);

  /* TIM8 enable counter */

  TIM_Cmd(TIM8, ENABLE);

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
pedro
Associate II
Posted on July 01, 2015 at 22:57

Thanks clive1!

I knew it had to be something simple that I was missing.