2011-06-02 3:23 AM
Hello,
i try get interrupt from timer 2 in compare mode. I want up count mode and generate interrupt in case match compare_register and counter and in case overflow counter. I'm using TrueStudio. Here is my code: void EXTI0_IRQHandler(void) { /*-----LOCAL-VARIABLES-----------------*/ int i=100000; if(EXTI_GetITStatus(USER_BUTTON_EXTI_LINE) != RESET) { if(k){SetFreqViaHSI(24);k=0;} else{SetFreqViaHSI(2);k=1;} while(i){i--;} /* Clear the User Button EXTI line pending bit */ EXTI_ClearITPendingBit(USER_BUTTON_EXTI_LINE); } } void TIM2_IRQHandler(void) { if(TIM2->SR&&TIM_SR_CC1IF){STM32vldiscovery_LEDOn(LED4);} else{STM32vldiscovery_LEDOn(LED4);} TIM2->SR=0x0000; TIM2->CR1|=0X0001; } /*-----MAIN-FUNCTION-------------------*/ int main(void) { /*-----LOCAL-VARIABLES-----------------*/ unsigned long int i=0; /*-----CONFIGURACE---------------------*/ SetFreqViaHSI(24); //set HSI and PLL to 24MHz STM32vldiscovery_LEDInit(LED3); //init LED3 (0) STM32vldiscovery_LEDInit(LED4); //init LED4 (1) STM32vldiscovery_LEDOn(LED3); STM32vldiscovery_LEDOff(LED4); RCC->APB1RSTR=RCC_APB1RSTR_TIM2RST; //peripheral reset RCC->APB2ENR=RCC_APB2ENR_IOPCEN; //portc Clock enable RCC->APB1ENR=RCC_APB1ENR_TIM2EN; //peripheral enable NVIC_EnableIRQ(TIM2_IRQn); //nvic configure TIM2->DIER=TIM_DIER_CC1IE|TIM_DIER_UIE; //enable interrupt TIM2->CCMR1=TIM_CCMR1_OC1M_0; TIM2->EGR=TIM_EGR_UG; //Update Generation TIM2->CCR1=0xBF; TIM2->CCER=TIM_CCER_CC1E; //Capture/Compare 1 output enable TIM2->CR1=TIM_CR1_CEN; //enable counter STM32vldiscovery_PBInit(BUTTON_USER, BUTTON_MODE_EXTI); // init button - interrupt /*-----MAIN-LOOP-----------------------*/ while (1) { } } void SetFreqViaHSI(int freq) { /* SYSCLK, HCLK, PCLK2 and PCLK1 configuration -----------------------------*/ int i=400; RCC_DeInit(); //default settings RCC_HSICmd(ENABLE); //enable HSI RCC_SYSCLKConfig(RCC_SYSCLKSource_HSI); //HSI - clock source while (RCC_GetSYSCLKSource() != 0x00) //check HSI is clock source { } while(i){i--;} //delay FLASH_SetLatency(FLASH_Latency_0); //flash 0 wait state RCC_HCLKConfig(RCC_SYSCLK_Div1); //HCLK = SYSCLK RCC_PCLK2Config(RCC_HCLK_Div1); //PCLK2 = HCLK RCC_PCLK1Config(RCC_HCLK_Div1); //PCLK1 = HCLK RCC_PLLConfig(RCC_PLLSource_HSI_Div2, RCC_PLLMul_6); RCC->CFGR&=0xFFFFFF0F; RCC->CFGR|=RCC_SYSCLK_Div1; RCC_PLLCmd(ENABLE); //Enable PLL while (RCC_GetFlagStatus(RCC_FLAG_PLLRDY) == RESET) //Wait till PLL is ready { } RCC_SYSCLKConfig(RCC_SYSCLKSource_PLLCLK); //Select PLL as system clock source while (RCC_GetSYSCLKSource() != 0x08) //Wait till PLL is used as system clock source { } } so that is it. I have breakpoint on ''void TIM2_IRQHandler(void)'' but it newer fall in tim2 interrupt. Do you see any mistake? or do you have some example, to study how to set timer and interrupt? thanks2011-06-02 10:01 AM
Do you see any mistake? or do you have some example, to study how to set timer and interrupt?
Several obvious flaws, and yes several examples have been posted on the forum. if(TIM2->SR&&TIM_SR_CC1IF){STM32vldiscovery_LEDOn(LED4);} else{STM32vldiscovery_LEDOn(LED4);} One too many ampersands there to do what you want. RCC->APB1RSTR=RCC_APB1RSTR_TIM2RST; //peripheral reset Holding TIM2 in reset, I think. Suggest you use the library, unless you enjoy debugging register minutia. If you want to use register directly, don't write in absolute values, mask in the bits you want to change.
2011-06-04 2:03 AM
so, you were right, ''RCC->APB1RSTR=RCC_APB1RSTR_TIM2RST;'' holded device in reset. Now it's working:
RCC->APB1RSTR|=RCC_APB1RSTR_TIM2RST; //peripheral reset RCC->APB1RSTR&=~RCC_APB1RSTR_TIM2RST; //peripheral reset off thanks