Associate III
April 23, 2014
Question
TIM_6Steps
- April 23, 2014
- 7 replies
- 1800 views
Posted on April 23, 2014 at 16:54
Hi all together,
I want to test the TIM_6Steps from the ''STM32F4xx_DSP_StdPeriph_Lib_V1.3.0'' Library with the STM32F4-Discovery-Board which uses the STM32F407VGT6. The compiler does not send any error but I do not get any output signal!!! I have added the code in the appendix. I only use the output PE11 instead of PA10 for TIM1 output Channel3. If someone of you has got any idea what I should do to get the program working, please let me know! Thank you. Best regards, Patrick