The Ultimate Capacitive Touch Sensor StackUp Guide
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2018-12-19 3:32 AM
As capacitive sensing undergoing such a rapid growth and penetrating more and more industries, it attracts the interest of many engineers with little to none experience with it.
That’s why, we have created this guide and we would like to share it with the ST community, PCAP design engineers and everyone that will have to include capacitive touch sensor designs in their systems! It provides you with insight on the anatomy of a capacitive touch sensor and industry terms, including:
1) Common stackup components
3) Attributes of common materials in the stackup
Plus: A table of all the materials of a StackUp and their dielectric constants
The stackup is the part of the touch sensor that the electrodes are enclosed within. It consists of multiple layers and its functionality is to protect the electrodes and help achieve the desired sensitivity of the sensor.
Apart from the electrodes, the rest of the elements that make up a touch sensor include:
1) Front Panel Material
2) Dielectrics
3) Adhesives
4) Air gaps
The front panel material is the material that is located at the top of the stackup. These materials provide protection to the sensor and should have a transparency of more than 90% if they are placed on top of screens.
Front Panel Material Required Properties:
1) Optical (e.g. transmittance, anti-haze, antiglare etc)
2) Mechanical (anti-scratch, drop resistance, anti-shatter)
The most common front panel materials are glass and plastic, though glass is mostly preferred.
The glass is a versatile material with multiple uses within the stackup. Its most common use is as a front panel material (also known as a cover glass), but it can also be used within the stackup. The main variables to consider when selecting a cover glass are its dielectric constant and its thickness.
The characteristics of the glass that make is such a good fit for many touch sensor applications include its high dielectric constant, its excellent optical properties and the mechanical structural integrity it offers. On the other hand, plastic has a worse dielectric constant and using it as a front cover material can result in a less sensitive sensor.
Dielectrics
Dielectrics can be used as substrates or as layers that help achieve the desired sensitivity of the sensor. A substrate is the base material that carries
the electrodes.
Even though any insulating material could be used as a substrate for capacitive sensing, low loss ones such as PET are preferred. Glass can also be used as a dielectric.
The main thing to consider when selecting dielectrics is their dielectric constant.
The rule of thumb here is: dielectrics placed between the driving and receiving electrodes (when they are in different layers) should have a lower dielectric constant and a higher one when they’re placed on either side of them. This stems from the underlying science and it has to do with improving the sensor’s sensitivity.
You can read our full guide in the link below.
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2018-12-19 6:50 AM
I appreciate that you give away some knowhow, but you should have identified this post as a promotion/ad, and perhaps ask the moderators for approval.
JW
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2018-12-19 7:11 AM
@Community member thank you for appreciating the value of our content and your kind observation.
Yes in my first post i asked for moderators if it's the right place or there is a better way as a blog post.
Since lots of PCAP designers have various questions, i think that the STM forum is the most right place to share that kind of content and help anyone that has PCAP design problems.